mm9z1_638 current accuracy is out of 1% requirement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mm9z1_638 current accuracy is out of 1% requirement

1,153 次查看
a852013777
Contributor III

Hi Nxp partner 

After we perform AN12301 calibration guide, we record the current reading from mm9z1_638. We found there are 3 to 5 reading is over our accuracy 1% requirement. Do you have any Low pass filter from software or hardware? How to determine the low pass cofficient?Do you reference guideline?

a852013777_1-1681716380417.png

 

a852013777_0-1681715601735.png

 

 

0 项奖励
回复
2 回复数

1,144 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mike,

Looking at the data, it seems there is some periodic lower reading, where is this coming from? Is this from the test equipment or SW?

Capture.JPG.png

Seems this periodic event is causing the issue.

Best regards,

Tomas

0 项奖励
回复

1,121 次查看
a852013777
Contributor III

Hi Tomas

 

Thanks, we chagne another electrical current source. the fail condition was fixed.

but we performed the 6A accuradcy can't meet +/-1%, The noise is about  100mA . Do you have suggestion reduce the 100mA noise ? or the 100mA noise is acceptable.

a852013777_0-1681982767855.png

 

Br,

Mike  Liang

 

0 项奖励
回复