Support for MMA8450 in MMA845X driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for MMA8450 in MMA845X driver?

ソリューションへジャンプ
1,275件の閲覧回数
Xavier
Contributor III

I need to add MMA8450 support in MMA845X official driver. Is there any patch or something to do that? Zhang Jiejing seemed to write the driver I need...

[lm-sensors] [PATCH] hwmod: sensors: mma845x gravity sensor chips

ラベル(1)
0 件の賞賛
返信
1 解決策
1,111件の閲覧回数
Xavier
Contributor III

Since I2C driver structures were pretty much the same I injected MMA8450 driver code into MMA845X driver thanks to a if statement after having identified the chip.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,112件の閲覧回数
Xavier
Contributor III

Since I2C driver structures were pretty much the same I injected MMA8450 driver code into MMA845X driver thanks to a if statement after having identified the chip.

0 件の賞賛
返信