Hello,
I would like to test the RD4247MAG3110 (eCompass kit with USB interface) for integration with my own measurement system (DotNet 4.0, Win7, 64bit). I know that there is the eCompass Software, but that is a standalone application. What I would need is some kind of software development kit, a description of the functions and interfaces included in the DLLs to create my own application (as part of the mentioned larger system). Some example code would also certainly help. C/C++ would be fine (I could write my own wrapper for C#)
Any help is appreciated
best regards
Sandro Guidati
已解决! 转到解答。
Sandro,
Actually, the eCompass/magnetic calibration solution is what you are after. Go to http://www.freescale.com/eCompass and click on the ECOMPASS_SW link on the bottom. After going through the clickthrough license, you'll be able to download a zip file which a whole bunch of app notes AND C source files.
Regards,
Mike
Sandro,
Actually, the eCompass/magnetic calibration solution is what you are after. Go to http://www.freescale.com/eCompass and click on the ECOMPASS_SW link on the bottom. After going through the clickthrough license, you'll be able to download a zip file which a whole bunch of app notes AND C source files.
Regards,
Mike
Hello Michael,
thanks for the quick response. I will have a look at the data.
I received my RD4247MAG3110 today, downloaded the sensortoolbox (to try the performance), installed the latest FTDI driver. The system is WIn7 64 bit. When I start the toolbox the sensors are detected, but when I press on "eCompass" I get a "class not registered" error. Do you have any idea, what I am missing?
regards
Sandro