NTM88 external sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NTM88 external sensor

515 次查看
Jpernia89
Contributor I

Hi guys,

I'll like to add a temperature sensor beside the one that this uC comes with. How can I do that? is there an option for one wire connection for interfacing a sensor like DS18B20? or how can i send a spi data to the NTM88 for RF transmitting (I'm thinking of connecting Low power uC with a sensor and sending it to the NTM88 via spi). Or the possibility to connect analog sensor to the NTM88.

 

 

0 项奖励
回复
2 回复数

438 次查看
Sebastian-Jaimes
Contributor I

Hello guys, I still got the question, if I want to add an external temperature sensor to the NTM88, but it has no IIC, is it posible to use the ADC that comes with the NTM88?

0 项奖励
回复

506 次查看
guoweisun
NXP TechSupport
NXP TechSupport

We don't have one wire connection temp sensor,but IIC interface instead.

I3C/I²C Digital Temperature Sensors | NXP Semiconductors

标记 (1)
0 项奖励
回复