Hi guys,
I'll like to add a temperature sensor beside the one that this uC comes with. How can I do that? is there an option for one wire connection for interfacing a sensor like DS18B20? or how can i send a spi data to the NTM88 for RF transmitting (I'm thinking of connecting Low power uC with a sensor and sending it to the NTM88 via spi). Or the possibility to connect analog sensor to the NTM88.
Hello guys, I still got the question, if I want to add an external temperature sensor to the NTM88, but it has no IIC, is it posible to use the ADC that comes with the NTM88?
We don't have one wire connection temp sensor,but IIC interface instead.