HI, i am using MPXV10GC6U sensor for my application vaccume pressure is the input , at 1inch of the pressure the sensor shows different output at every time , how to tackle this ????
thank you in
this is the interface i have used please guide me
advance
Hello kumod,
I hope all is great with you. Thank you for using the NXP communities.
Please note that this is an uncompensated device. it means that the properties of the strain gauge itself are temperature dependent, requiring that the device be temperature compensated if it is to be used over an extensive temperature range.
Temperature compensation and offset calibration can be achieved rather simply with additional resistive components, or by designing your system using the MPX2010 series sensor.
You may review the application note below for further information.
Temperature compensation methods
I hope this information helps.
Regards,
David
Hello kumod,
I am pleased to contact you again.
I recommend considering the following circuit for the signal conditioning. Such a circuit incorporates both span and offset temperature compensation.
I hope this information will be useful for you.
Regards,
David