imx8mp with sony imx412 and 4 lanes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp with sony imx412 and 4 lanes

1,012 Views
pmliquify
Contributor II

Hi all, 

Situation:

I developed drivers for the sony imx412 and imx327 camera modules. Both cameras are working fine with 2 lanes. The imx327 additionally works fine with 4 lanes. All tests are done on both camera ports of the imx8mp. 

See my device tree files attached!

 

imx8mp.dtsi
+-> imx8mp-var-dart.dtsi
    +-> imx8mp-var-dart-dt8mcustomboard.dts
        +-> imx8mp-var-dart-dt8mcustomboard-vc-mipi-isi0.dts

 

Problem:

The imx412 doesn't even start streaming with 4 lanes. On neither camera port. Sometimes I get a first image. After that the stream stops and never delivers a second image. This first image contains half of all data. The bayer pattern seems "broken". I guess this is because only every second line of the image is transmitted.

imx8mp_IMX412_4Lanes.png

Update: My latest tests

  • Sony IMX412 from Vision Components on Variscite imx8mp Evaluation Kit, Kernel 5.15.71
  • 2 + 4 lanes always with pixelformat RG10

With 2 lanes I do get valid images with full resolution 4032x3040 and also with smaller resolutions. Everything is fine with 2 lanes.

With 4 lanes I found that I get valid images up to an image resolution of 2780x3040. When I increase the image width to 2781 and above the image isn't valid anymore. See example images.

20240313-110129_lowres.png20240313-110757_lowres.png

In all cases I do get following log

 

mxc-mipi-csi2.0: Frame End events: 2
mxc-mipi-csi2.0: Frame Start events: 2
mxc-mipi-csi2.0: Non-image data after odd frame events: 0
mxc-mipi-csi2.0: Non-image data before odd frame events: 0
mxc-mipi-csi2.0: Non-image data after even frame events: 0
mxc-mipi-csi2.0: Non-image data before even frame events: 0
mxc-mipi-csi2.0: Unknown Error events: 0
mxc-mipi-csi2.0: CRC Error events: 0
mxc-mipi-csi2.0: ECC Error events: 0
mxc-mipi-csi2.0: FIFO Overflow Error events: 0
mxc-mipi-csi2.0: Lost Frame End Error events: 0
mxc-mipi-csi2.0: Lost Frame Start Error events: 0
mxc-mipi-csi2.0: SOT Error events: 0

 

This leads me to believe, that the CSI receiver works fine, but the ISI is doing something bad.
Any suggestions?

0 Kudos
12 Replies

753 Views
pmliquify
Contributor II

Any help is highly appreciated. Any suggestions or advice on how to analyze the problem?

0 Kudos

741 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try the settings I suggest to you one week ago?

0 Kudos

825 Views
pmliquify
Contributor II

Update: My latest tests

  • Sony IMX412 from Vision Components on Variscite imx8mp Evaluation Kit, Kernel 5.15.71
  • 2 + 4 lanes always with pixelformat RG10

With 2 lanes I do get valid images with full resolution 4032x3040 and also with smaller resolutions. Everything is fine with 2 lanes.

With 4 lanes I found that I get valid images up to an image resolution of 2780x3040. When I increase the image width to 2781 and above the image isn't valid anymore. See example images.

20240313-110129_lowres.png 20240313-110757_lowres.png

In all cases I do get following log

 

mxc-mipi-csi2.0: Frame End events: 2
mxc-mipi-csi2.0: Frame Start events: 2
mxc-mipi-csi2.0: Non-image data after odd frame events: 0
mxc-mipi-csi2.0: Non-image data before odd frame events: 0
mxc-mipi-csi2.0: Non-image data after even frame events: 0
mxc-mipi-csi2.0: Non-image data before even frame events: 0
mxc-mipi-csi2.0: Unknown Error events: 0
mxc-mipi-csi2.0: CRC Error events: 0
mxc-mipi-csi2.0: ECC Error events: 0
mxc-mipi-csi2.0: FIFO Overflow Error events: 0
mxc-mipi-csi2.0: Lost Frame End Error events: 0
mxc-mipi-csi2.0: Lost Frame Start Error events: 0
mxc-mipi-csi2.0: SOT Error events: 0

 

This leads me to believe, that the CSI receiver works fine, but the ISI is doing something bad.
Any suggestions?

0 Kudos

973 Views
joanxie
NXP TechSupport
NXP TechSupport

could you share

imx8mp-var-dart-dt8mcustomboard.dts

and all of other include dtsi files? check if the clock is available for 4 data lane

0 Kudos

966 Views
pmliquify
Contributor II

Yes of coarse, I attached the files to my first post. See above.

0 Kudos

937 Views
joanxie
NXP TechSupport
NXP TechSupport

what format do you use for capture? not raw data? and what command do you use to capture the data from imx412?

0 Kudos

930 Views
pmliquify
Contributor II

I do capture images with RAW10 (RG10) pixelformat. The screenshot is created with my self develop test app (https://github.com/pmliquify/v4l2-test). The test app debayers the image with opencv. 

But I do get the capture problem as well with v4l2-ctl.

0 Kudos

859 Views
joanxie
NXP TechSupport
NXP TechSupport

since you use raw data, why don't you use ISP for this? if you need to use ISI, do you add raw10 format in the ISI driver?

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/staging/media/imx/imx8-isi-fmt.c

0 Kudos

852 Views
pmliquify
Contributor II
Hi joanxie,

I will use the ISP once the system delivers images via the v4l2 interface. My current problem is, that I do not receive images in memory with the IMX412 and 4 lanes. I DO get images with 2 lanes but NOT with 4 lanes.
  • Which possibilities exist to debug my system?
  • How is it possible to see/debug if the csi receivers receives data?
  • How is it possible to see if the isi is receiving data?
  • Is it possible that I do not receive data, because of wrong csis-hs-settle, csis-clk-settle settings? How to determine the correct settings?
Any help is highly appreciated!
0 Kudos

836 Views
joanxie
NXP TechSupport
NXP TechSupport

for 2 data lane and 4 data lane, do you use the same video format, resolution? just change the data lane from 2 to 4? could you give me the logfile when you use capture command with data lane 4? also pls dump the mipi csi registers to check, for csis-hs-settle, csis-clk-settle, which is depends on your actual mipi frequency, you can try to set csis-hs-settle = <16>;

0 Kudos

585 Views
pmliquify
Contributor II

I set csis-hs-settle = <16>; => No success.

Here is the reg dump for 2 lanes:

 

vc-mipi-cam 1-001a: vc_sen_set_binning_mode(): Set binning mode: 0
vc-mipi-cam 1-001a: vc_core_set_format(): Set format 0x300f (RG10)
vc-mipi-cam 1-001a: vc_core_try_format(): Try format 0x300f (RG10, format: 0x2b)
vc-mipi-cam 1-001a: vc_core_set_frame_size(): Set frame size (width: 4032, height: 3040)
vc-mipi-cam 1-001a: vc_core_get_format(): Get format 0x300f (RG10)
vc-mipi-cam 1-001a: vc_core_get_frame(): Get frame (width: 4032, height: 3040)
bypass csc
input fmt RGB4
output fmt RG10
i2c 1-0010: vc_mod_set_mode(): Set module mode: 0 (lanes: 2, format: RG10, type: STREAM)
i2c 1-0010: vc_mod_set_power(): Set module power: down
i2c 1-0010: vc_mod_set_power(): Set module power: up
vc-mipi-cam 1-001a: vc_sen_set_exposure(): Set sensor exposure: 10000 us
vc-mipi-cam 1-001a: vc_sen_set_gain(): Set sensor gain: 0
vc-mipi-cam 1-001a: vc_sen_set_blacklevel(): Set sensor black level: 64
vc-mipi-cam 1-001a: vc_sen_start_stream(): Start streaming
mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0
vc-mipi-cam 1-001a: vc_core_get_format(): Get format 0x300f (RG10)
mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset: bus fmt is 10 bit !
mxc-mipi-csi2.0: fmt: 0x300f, 4032 x 3040
mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
mxc-mipi-csi2.0:         CSIS_VERSION[0]: 0x03060301
mxc-mipi-csi2.0:        CSIS_CMN_CTRL[4]: 0x00004905
mxc-mipi-csi2.0:        CSIS_CLK_CTRL[8]: 0x000f0000
mxc-mipi-csi2.0:          CSIS_INTMSK[10]: 0x0fffff1f
mxc-mipi-csi2.0:          CSIS_INTSRC[14]: 0x00000000
mxc-mipi-csi2.0:      CSIS_DPHYSTATUS[20]: 0x000000c0
mxc-mipi-csi2.0:        CSIS_DPHYCTRL[24]: 0x10800007
mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_L[30]: 0x000001f4
mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_H[34]: 0x00000000
mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_L[38]: 0x00000000
mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_H[3c]: 0x00000000
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH0[40]: 0x000000ac
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH1[50]: 0x000008fd
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH2[60]: 0x000008fe
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH3[70]: 0x000008ff
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH0[44]: 0x0be00fc0
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH1[54]: 0x80008000
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH2[64]: 0x80008000
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH3[74]: 0x80008000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH0[48]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH1[58]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH2[68]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH3[78]: 0x00000000
mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
mxc-mipi-csi2.0:    GPR_GASKET_0_CTRL[60]: 0x00000000
mxc-mipi-csi2.0:   GPR_GASKET_0_HSIZE[64]: 0x00000000
mxc-mipi-csi2.0:   GPR_GASKET_0_VSIZE[68]: 0x00000000
vc-mipi-cam 1-001a: vc_sen_stop_stream(): Stop streaming
mxc-mipi-csi2.0: mipi_csis_s_stream: 0, state: 0x0
mxc-mipi-csi2.0: Frame End events: 5
mxc-mipi-csi2.0: Frame Start events: 5
mxc-mipi-csi2.0: Non-image data after odd frame events: 0
mxc-mipi-csi2.0: Non-image data before odd frame events: 0
mxc-mipi-csi2.0: Non-image data after even frame events: 0
mxc-mipi-csi2.0: Non-image data before even frame events: 0
mxc-mipi-csi2.0: Unknown Error events: 0
mxc-mipi-csi2.0: CRC Error events: 0
mxc-mipi-csi2.0: ECC Error events: 0
mxc-mipi-csi2.0: FIFO Overflow Error events: 0
mxc-mipi-csi2.0: Lost Frame End Error events: 0
mxc-mipi-csi2.0: Lost Frame Start Error events: 1190
mxc-mipi-csi2.0: SOT Error events: 1

 

 And for 4 lanes:

 

vc-mipi-cam 1-001a: vc_sen_set_binning_mode(): Set binning mode: 0
vc-mipi-cam 1-001a: vc_core_set_format(): Set format 0x300f (RG10)
vc-mipi-cam 1-001a: vc_core_try_format(): Try format 0x300f (RG10, format: 0x2b)
vc-mipi-cam 1-001a: vc_core_set_frame_size(): Set frame size (width: 4032, height: 3040)
vc-mipi-cam 1-001a: vc_core_get_format(): Get format 0x300f (RG10)
vc-mipi-cam 1-001a: vc_core_get_frame(): Get frame (width: 4032, height: 3040)
bypass csc
input fmt RGB4
output fmt RG10
i2c 1-0010: vc_mod_set_mode(): Set module mode: 1 (lanes: 4, format: RG10, type: STREAM)
i2c 1-0010: vc_mod_set_power(): Set module power: down
i2c 1-0010: vc_mod_set_power(): Set module power: up
vc-mipi-cam 1-001a: vc_sen_set_exposure(): Set sensor exposure: 10000 us
vc-mipi-cam 1-001a: vc_sen_set_gain(): Set sensor gain: 0
vc-mipi-cam 1-001a: vc_sen_set_blacklevel(): Set sensor black level: 64
vc-mipi-cam 1-001a: vc_sen_start_stream(): Start streaming
mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0
vc-mipi-cam 1-001a: vc_core_get_format(): Get format 0x300f (RG10)
mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset: bus fmt is 10 bit !
mxc-mipi-csi2.0: fmt: 0x300f, 4032 x 3040
mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
mxc-mipi-csi2.0:         CSIS_VERSION[0]: 0x03060301
mxc-mipi-csi2.0:        CSIS_CMN_CTRL[4]: 0x00004b05
mxc-mipi-csi2.0:        CSIS_CLK_CTRL[8]: 0x000f0000
mxc-mipi-csi2.0:          CSIS_INTMSK[10]: 0x0fffff1f
mxc-mipi-csi2.0:          CSIS_INTSRC[14]: 0x00000000
mxc-mipi-csi2.0:      CSIS_DPHYSTATUS[20]: 0x00000000
mxc-mipi-csi2.0:        CSIS_DPHYCTRL[24]: 0x1080001f
mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_L[30]: 0x000001f4
mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_H[34]: 0x00000000
mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_L[38]: 0x00000000
mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_H[3c]: 0x00000000
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH0[40]: 0x000000ac
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH1[50]: 0x000008fd
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH2[60]: 0x000008fe
mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH3[70]: 0x000008ff
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH0[44]: 0x0be00fc0
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH1[54]: 0x80008000
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH2[64]: 0x80008000
mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH3[74]: 0x80008000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH0[48]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH1[58]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH2[68]: 0x00000000
mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH3[78]: 0x00000000
mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
mxc-mipi-csi2.0:    GPR_GASKET_0_CTRL[60]: 0x00000000
mxc-mipi-csi2.0:   GPR_GASKET_0_HSIZE[64]: 0x00000000
mxc-mipi-csi2.0:   GPR_GASKET_0_VSIZE[68]: 0x00000000
vc-mipi-cam 1-001a: vc_sen_stop_stream(): Stop streaming
mxc-mipi-csi2.0: mipi_csis_s_stream: 0, state: 0x0
mxc-mipi-csi2.0: Frame End events: 8
mxc-mipi-csi2.0: Frame Start events: 8
mxc-mipi-csi2.0: Non-image data after odd frame events: 0
mxc-mipi-csi2.0: Non-image data before odd frame events: 0
mxc-mipi-csi2.0: Non-image data after even frame events: 0
mxc-mipi-csi2.0: Non-image data before even frame events: 0
mxc-mipi-csi2.0: Unknown Error events: 0
mxc-mipi-csi2.0: CRC Error events: 0
mxc-mipi-csi2.0: ECC Error events: 1
mxc-mipi-csi2.0: FIFO Overflow Error events: 0
mxc-mipi-csi2.0: Lost Frame End Error events: 0
mxc-mipi-csi2.0: Lost Frame Start Error events: 1342
mxc-mipi-csi2.0: SOT Error events: 1

 

0 Kudos

555 Views
joanxie
NXP TechSupport
NXP TechSupport

you said your IMX412 can work with 2 lane, but why the dump error message for 2 lane settings? and pls check the register Gasket 0 Control Register (GASKET_0_CTRL), this register shouldn't be 0, you should set correct format for your camera, so pls check it

0 Kudos