MPXM2102AS Supply Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXM2102AS Supply Voltage

ソリューションへジャンプ
641件の閲覧回数
leonardorossi
Contributor I

I would like to know what would be the consequences of feeding in 12V straight into this pressure sensor. The datasheet states a typical value of 10V, but a max of 16V. I don't want to regulate 10V in my system exclusively for this sensor, so will it work properly under 12V?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
549件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Leonardo,

Yes, it will without any problems. The MPXM2102AS is ratiometric so its sensitivity varies proportionally to the supply voltage. When powered by 12V, the sensitivity will be 0.4mV/kPa * 12V / 10V = 0.48mV/kPa.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
550件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Leonardo,

Yes, it will without any problems. The MPXM2102AS is ratiometric so its sensitivity varies proportionally to the supply voltage. When powered by 12V, the sensitivity will be 0.4mV/kPa * 12V / 10V = 0.48mV/kPa.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信