MMA8451 Termic Drift

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451 Termic Drift

701件の閲覧回数
umbertogrechi
Contributor I

Hi, i'm using a MMA8451 accelerometer as inclinometer for external application, i've seen that the variations of temperature affects the measures. There are standard parameters to correct the measure?

Unfortunately i don't have the opportunity to test the sensor at different temperatures in order to find the necessary parameters.

Best regards,

Umberto


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 件の賞賛
返信
1 返信

512件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Umberto,

Thank you for writing.

As you may know, the offset error might be caused by the situations listed below:

- Device to device variations.
- Mechanical stress from packaging and mounting.
- Shifts due to temperature and aging.

In order to correct the measure, I recommend to use our software technique "AutoZero".


If you are repeatedly using AutoZero during initialization, to compensate for offset drift, etc. You won’t require offset calibration, hence the accuracy of the device would be highly improved (including repeatability).

As for Zero-g offset, it is necessary to do a calibration to exactly know what the offset is.  Please look at AN3447 “Implementing Auto-Zero Calibration Technique for Accelerometers", it was written for the MMA7455L, but the principle is the same, hence you can apply the same technique to the MMA5481:

Implementing Auto-Zero Calibration Technique for Accelerometers

 

Please let me know if this information helps.

Regards,

David

0 件の賞賛
返信