MM9Z1_638 Zero voltage and Zero Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1_638 Zero voltage and Zero Current

ソリューションへジャンプ
618件の閲覧回数
a852013777
Contributor III

Hi NXP partner

We use MM9Z1_638 to be battery junction box senor board.When we apply 0V and 0A to mm9z1_638 senor board A~H point which show test configuration file. We found mm9z1_638 report  is 0~1.2V and 0~0.1A through CANBUS. as attached file. How to etiminate the minor voltage and current when our voltage sensor point and current senor with 0V and 0A.

Br,

Mike Liang

 

0 件の賞賛
返信
1 解決策
609件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mike,

please refer to the AN12301. There is a possibility of VSENSE, ISENSE and TSENSE calibration. In the section 5. is the description of the system calibration procedure.

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
610件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mike,

please refer to the AN12301. There is a possibility of VSENSE, ISENSE and TSENSE calibration. In the section 5. is the description of the system calibration procedure.

With Best Regards,

Jozef

0 件の賞賛
返信