Fxps7400 Part number

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fxps7400 Part number

Jump to solution
1,813 Views
francoisdugue
Contributor III

Hi,

Working on the pressure sensor Fxps7400, using I2C, I have download sample code of Fxpss7400 Sensor Driver.

I have some question regarding the initialization.

 

uint8_t fxps7xxx_init(fxps7xxx_driver_t *pDriver)
{
  // Initial the sensor driver handler and interfaces
    if(NULL == pDriver){
        return SENSOR_INVALIDPARAM_ERR;
    } 
    uint8_t status = SENSOR_SUCCESS;
    // initialize the communication channel
    status = sensor_comm_init(&pDriver->comHandle);
    if(status != SENSOR_SUCCESS){
    	return status;
    }

    uint8_t data = 0;
    // dummy read to flush the data in communication buffer
    sensor_comm_read(&pDriver->comHandle, FXPS7XXX_DEVSTAT, sizeof(data), &data);

	status = sensor_comm_read(&pDriver->comHandle, FXPS7XXX_WHO_AM_I, sizeof(data), &data);

	if(data != FXPS7XXX_H_WHOAMI_VALUE){
		return FXPS7XXX_DEVICE_NOT_FOUND;
	}

	status  = load_region(pDriver, CONFIG_C_REGSITERS);
	if(status != SENSOR_SUCCESS){
		return status;
	}
	//read the part information
	uint8_t part_data = 0;
	uint8_t part_index = 0;
	status = sensor_comm_read(&pDriver->comHandle, FXPS7XXX_PN1, sizeof(part_data), &part_data);
    if(part_data == 0x16){
        part_index = 0;
    }else{
        part_index = (part_data>>4 & 0x0F);
    }
	pDriver->pressureOffset = part_tbl[part_index].pabOffSet;
	pDriver->pressureSensitivity = part_tbl[part_index].pabSense;
	return status;
}

 

First, it checks if the right part is present, with the good WhoAmI value.

Then is load specific memory region. I think it is necessary to be able to read the PN. Can you firm?

Reading PN register, it uses it as index of a table to obtain some parameters.

 

// fxps7xxx part information table
const fxps7xxx_part_table_t part_tbl[] = {{0x16,  24939.7, 66.62},
{0x11,  25536.4, 93.34},
{0x25, 28661.6, 30.42},
{0x0,  0, 0},		//dummy
{0x40, 28900, 14},
{0x55, 28990, 14}};

 

When I execute this on my device, I get over I2C [0x0C;0x40] ...

Can you explain me the link between device part number (normally FXPS7400DIA4) and the one i get from the device?

The part number registers are factory programmed OTP registers that include the
numeric portion of the device part number.

Can you tell me if I shall reuse or update the data from the part_tbl[] according to my device?

thanks in advance

Francois

Labels (1)
0 Kudos
Reply
1 Solution
1,758 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Francois,

please see below answers from an application engineer I have contacted.

DESCRIPTION

  1. Have we to load region to be able to read the PN?
  2. How the PN that I received [0x0C;0x40] is linked to my device part number (FXPS7400DIA4)

[A] For items 1, 2: The customer is reading the correct values.  The values for these two registers should be: C4 = 0C and C5 = 40.  So when you read them sequentially you get 400C where the 400 means 20kPa to 400kPa device (FXPS7400DI) and the C means it the I2C device.  Yes, the region has to be loaded and is correct as the customer shows.

3. Is the partNo list, from the part_tbl[], is complete or can I have a new value?

[A] For item 3: If I am understanding the customers question correctly, the part number table is complete.  Let me know otherwise.

4. Is the pabOffSet/pabSense from the part_tbl[] have to be adjusted trough a calibration process? 

[A] For item 4:  These values are fixed based on the device part number and are located in the scaling parameters table of the datasheet.  Always check the latest datasheet for correct settings.

With Best Regards,

Jozef

View solution in original post

6 Replies
1,804 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Francois,

could you please provide reading from the WHO_AM_I register? In a scope from an oscilloscope or from a logic analyzer? When you read the WHO_AM_I register, you should read the 0xC4 value. 

JozefKozon_0-1669813946559.png

JozefKozon_1-1669814061164.png

With Best Regards,

Jozef

0 Kudos
Reply
1,797 Views
francoisdugue
Contributor III

Hi Joseph,

Yes you're right the return is xC4.

I'm using Logic analyzer from Saleae, inc.

I can only share to you the logs because of Network policy...

The following logs show the execution of 

(void)fxps7xxx_init();
(void)fxps7xxx_get_pressure_temperature(&f32Pressure, &u8Temperature);

And as you can see, it return 0xC4.

write to 0x60 ack data: 0x3E 
read to 0x60 ack data: 0xC4
write to 0x60 ack data: 0x14 0xC0 
write to 0x60 ack data: 0x15 
read to 0x60 ack data: 0xC0
write to 0x60 ack data: 0xC4 
read to 0x60 ack data: 0x0C 0x40
write to 0x60 ack data: 0x62 
read to 0x60 ack data: 0xA3 0x76
write to 0x60 ack data: 0x0E 
read to 0x60 ack data: 0x5E

 

1,791 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Francois,

thank you for your answer. Great, so you are receiving correct value from the WHO_AM_I register.

With Best Regards,

Jozef

0 Kudos
Reply
1,787 Views
francoisdugue
Contributor III

Hello Jozef, thank you for your quickness.

Indeed I2C exchanges are correct and i have the right device, but this was not my questions

I try to understand the initialization function from the example...

  • Have we to load region to be able to read the PN?
  • How the PN that I received [0x0C;0x40] is linked to my device part number (FXPS7400DIA4)
  • Is the partNo list, from the part_tbl[], is complete or can i have a new value?
  • Is the pabOffSet/pabSense from the part_tbl[] have to be adjusted trough a calibration process? 

Thank in advance for these answers.

Regards,

François

0 Kudos
Reply
1,759 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Francois,

please see below answers from an application engineer I have contacted.

DESCRIPTION

  1. Have we to load region to be able to read the PN?
  2. How the PN that I received [0x0C;0x40] is linked to my device part number (FXPS7400DIA4)

[A] For items 1, 2: The customer is reading the correct values.  The values for these two registers should be: C4 = 0C and C5 = 40.  So when you read them sequentially you get 400C where the 400 means 20kPa to 400kPa device (FXPS7400DI) and the C means it the I2C device.  Yes, the region has to be loaded and is correct as the customer shows.

3. Is the partNo list, from the part_tbl[], is complete or can I have a new value?

[A] For item 3: If I am understanding the customers question correctly, the part number table is complete.  Let me know otherwise.

4. Is the pabOffSet/pabSense from the part_tbl[] have to be adjusted trough a calibration process? 

[A] For item 4:  These values are fixed based on the device part number and are located in the scaling parameters table of the datasheet.  Always check the latest datasheet for correct settings.

With Best Regards,

Jozef

1,752 Views
francoisdugue
Contributor III
Hi;
Ok thank you for your support
Regards.