S32V234 Camera Sensor and Deserializer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32V234 Camera Sensor and Deserializer

622 次查看
rafe_ma
Contributor I

Current development environment and purpose:
1. The version number of the development board is: SVM_HD_S32V234_V2.0_20180110
2. We want to use the external frame sync mode to calculate the delay stability of the transmission link from the camera sensor to the DDR buffer.

Questions:
1. Does the hardware support the external frame sync mode?
2. Which pin is the SOC connected to the MAX9286? Is there a schematic diagram of this part available?
3. If the hardware supports it, is there any corresponding document on the software for reference?
4. If the hardware does not support it, how can the jumper solve this problem?

标记 (1)
0 项奖励
回复
0 回复数