静态气压测试值变为11K左右(不良)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

静态气压测试值变为11K左右(不良)

938 Views
zhanglei2015xx
Contributor II

无人机项目上使用MP3H6115AC6T1(NXP)压力传感器,
100台机器正常SMT后测试静态气压为110K左右(正常),
但PCB板在经过组装后,有4台静态气压测试值变为11K左右(不良),
请问什么原因可能会导致此不良的产生。

Labels (1)
0 Kudos
Reply
1 Reply

801 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Our support engineers are located worldwide, therefore for a better understanding of your question, we suggest you continue the communication in English, meanwhile I will try to answer to your inquiry.

 

If I understand properly (please correct me if my understanding of the problem is wrong), you are applying a pressure of 110kPa on the sensor’s port before soldering it to the board for test purposes and it properly reads 100kPa (around 2.75V). And after assemble the pressure sensor t the board, you are applying the same 100kPa but reading only around 11kPa (around 0.125V). Is my understanding correct?

 

Seems like the pressure sensor is damaging during the assembly process, care must be taken when assembly this kind of sensor to the board, for example, you have to take in mind the following aspects:

* Handling of the sensor: You cannot apply vacuum to the sensor’s port during the pick and place of the sensor from the carrier tape to the board.

Check the App Note AN1984: https://www.nxp.com/docs/en/application-note/AN1984.pdf

 

* Soldering and cleaning: Exposed cavity packages like the MP3H6115AC6T1, require special considerations during board assembly to prevent damage to the device during soldering and subsequent cleaning operations.

Check the App Note AN3150: https://www.nxp.com/docs/en/application-note/AN3150.pdf


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply