Why APDU Command VERIFY returns 6a88

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why APDU Command VERIFY returns 6a88

4,850件の閲覧回数
michgomo08_2
Contributor I

I  am trying to run the VERIFY APDU command but the result is 6a88 (Referenced data not found).

My PIN is "012345" and based on some examples my command APDU is:

00 20 00 00 06 30 31 32 33 34 35

I hope the answer is 9000 but it is 6a88

The Card used is a NXP smard card similary to this.

The vendor of the reader recommended me to look for documentation on the card, and that before executing the verify command I had to execute the select command and other information, but honestly I did not understand this very well.

I wanted to know if you have any documentation that can help me.

I really appreciate in advance any help you can give me.

Regards.

タグ(3)
0 件の賞賛
返信
1 返信

4,739件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Michael Gomez,

Hope you are doing great, as you may know this type of devices ( SmartMX and JCOP ) are under NDA ( Non Disclosure Agreement) this means that all the information, tools and support should be delivered using secured communication channels and only to customers with active NDA. since this is a public forum we cannot discuss the behavior of such devices,  it is needed that you contact the company that sold you the cards  or the Sales form NXP that helped you to get them.

BR

Jonathan

0 件の賞賛
返信