S32K3 Safety Manual Addendum ID 1248005

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Safety Manual Addendum ID 1248005

ソリューションへジャンプ
649件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

In the Safety Manual Addendum there is an assumption with ID 1248005 that the TEST input is tied to ground during boot and normal operation mode.

The question is what Test input or Test pin is this referring to?

Thank you,

John H. Floros

0 件の賞賛
1 解決策
601件の閲覧回数
nxf55526
NXP Employee
NXP Employee

Hello John,

This assumption ID 1248005 has been removed from the updated list of assumptions since the S32K3 doesn't include a Test input pin. This would get reflected in the next draft of the Safety Manual. Hope this clarifies. 

Thanks and Regards,

Avni

元の投稿で解決策を見る

0 件の賞賛
1 返信
602件の閲覧回数
nxf55526
NXP Employee
NXP Employee

Hello John,

This assumption ID 1248005 has been removed from the updated list of assumptions since the S32K3 doesn't include a Test input pin. This would get reflected in the next draft of the Safety Manual. Hope this clarifies. 

Thanks and Regards,

Avni

0 件の賞賛