About the FIT rate of PMC Block of FS32K146

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the FIT rate of PMC Block of FS32K146

跳至解决方案
452 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi experts.

       I have encountered a problem raised by a customer, I hope experts in this field can give me some help, the case number is: 00442292 and thank you advance.

[Question]
Could you provide FIT Rate information of PMC Block? (I would like to know about the following two.)
1. FIT Rate information of PMC Block
2. FIT Rate information of LVD Block alone in PMC Block

[Background]
My customer want use Low voltage detect (LVD) in PMC Block for system reset sources,
so, they want know those FIT Rate.

[Refer to Reference Manual S32K-RM.pdf]
- p.535 : 25.2.2.2 Low voltage detect (LVD)
- p.560 : Clock definitions

Senlent_1-1642065073266.png

 

BR!

     Jim,

 

 

0 项奖励
1 解答
422 次查看
nxf61080
NXP Employee
NXP Employee

Hi Jim,

The following information can be found in Power_Internal_FMEDA workbook, and is TR62380 compliant.

1. FIT rate information for the PMC block: FMEDA sheet, T3: 6.05E-09
              Area for PMC can be found in the block and block sizes sheet: 156,583

2. . FIT rate information for the LVD block in PMC: FMEDA sheet: J222: 8.09E-16 h¯¹
              Area for LVD can be found in the block and block sizes sheet: 9,940

Thanks and regards,
Manibha

在原帖中查看解决方案

0 项奖励
1 回复
423 次查看
nxf61080
NXP Employee
NXP Employee

Hi Jim,

The following information can be found in Power_Internal_FMEDA workbook, and is TR62380 compliant.

1. FIT rate information for the PMC block: FMEDA sheet, T3: 6.05E-09
              Area for PMC can be found in the block and block sizes sheet: 156,583

2. . FIT rate information for the LVD block in PMC: FMEDA sheet: J222: 8.09E-16 h¯¹
              Area for LVD can be found in the block and block sizes sheet: 9,940

Thanks and regards,
Manibha

0 项奖励