why RTI interrupt can't triggle.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why RTI interrupt can't triggle.

ソリューションへジャンプ
1,271件の閲覧回数
KerryJ
Contributor II

I used the S32DS 3.4, Why PIT0_CH0 and PIT0_CH1 can generate a interrupt with the same configuration , but the PIT0_CH_RTI not?

0 件の賞賛
返信
1 解決策
1,218件の閲覧回数
nxf78987
NXP Employee
NXP Employee

Hi KerryJ,

This is an example, that you are needing.

Best regards,

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,254件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which device and which SDK/RTD is used?

Regards

Lukas

0 件の賞賛
返信
1,245件の閲覧回数
KerryJ
Contributor II

DEVICE IS

S32K344

AND RTD IS 

S32K3 RTD AUTOSAR 4.4 VERSION 2.0.0

0 件の賞賛
返信
1,219件の閲覧回数
nxf78987
NXP Employee
NXP Employee

Hi KerryJ,

This is an example, that you are needing.

Best regards,

Dan

0 件の賞賛
返信
1,200件の閲覧回数
KerryJ
Contributor II

Thanks you so much.

I find when I config PIT0_CH0 first, the PIT0_RTI is disabled, even though config RTI later, the RTI is still disabled.

You should config RTI first then config PIT0_CH0, which both RTI and CH_0 are useful.

タグ(1)
0 件の賞賛
返信