s32k3 SHE Basic secure boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k3 SHE Basic secure boot

跳至解决方案
826 次查看
luhaiou_autolink
Contributor I

I've been debugging the secureboot feature with s32k312 recently,

first debugging the Advance secure boot feature, it jumps from HSE_FW to app normally.

Now try to debug the Basic secure boot feature on the same machine.

My understanding is that I need to clear all the SMRs and CRs that I have installed before, so that I can debug the Basic secure boot normally,

luhaiou_autolink_0-1708420202808.png

 

Then how to format the installed SMRs and CRs?

0 项奖励
回复
1 解答
797 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @luhaiou_autolink 

if you still have the device in CUST_DEL life cycle, you can use following service to erase whole HSE data flash, so you can start over:

lukaszadrapa_0-1708459226716.png

Another option is to erase the entries individually:

lukaszadrapa_1-1708459356502.pnglukaszadrapa_2-1708459364618.png

Or you can remove the firmware completely and start over:

lukaszadrapa_3-1708459475785.png

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
1 回复
798 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @luhaiou_autolink 

if you still have the device in CUST_DEL life cycle, you can use following service to erase whole HSE data flash, so you can start over:

lukaszadrapa_0-1708459226716.png

Another option is to erase the entries individually:

lukaszadrapa_1-1708459356502.pnglukaszadrapa_2-1708459364618.png

Or you can remove the firmware completely and start over:

lukaszadrapa_3-1708459475785.png

Regards,

Lukas

0 项奖励
回复