Hi all:
by following the link in AUTOSAR Software|NXP , i got the news about "AUTOSAR Starter Kit for Arm Cortex S32K MCUs" ARCCORE - News . then i bought the S32K144-EVB for studying the autosar development .
i encountered some issues when i try to load the examples provided by the "S32K_StarterKit_2_0_1" package .
i don't know who will be the owner for the trouble fix ? NXP or ARC CORE ?
if NXP takes the ownership , please help me to fix below issues. thanks !!
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
i obtained the MCAL from NXP and the tresos studio from EB . now i am running the “HelloWorld_S32K14X Example".
as mentioned by the "Arccore HelloWorld GettingStarted_2.0.1.pdf", i need a CAN probe to run the example .
for i am a beginner in AUTOSAR and CAN development , could you recommend the "CAN Probe" which you are using ?
BTW, do you have the example project with a CAN device connected or with two starterkist exchanged the data via CAN bus ?
if yes, could you provide the project files and the webshop URL of the CAN device ?
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Dear Sadan when I setup the Tresos V23.0.0 it gives me same error that you got already.
The error says "No packages were found that can be installed!"
Best regards.
Merhaba,
Sanırım Türkçe yanıt verebilirim. Umarın NXP engellemez :smileyhappy:
Ben yaşadıoğım derleme problemlerine çözüm bulamadığım için ara verdim. Ne NXP'den ne Arccore firmasından ne de EB firmasından bir cevap alamadım. Hepsi topu birbirine attı ve çözümsüz kaldım.
Eğer bir çözüm bulursanız ve paylaşırsanız memnun olurum.
Özel değilse, hangi firmada çalışıyorsunuz? Nasıl bir projede kullanacaksınız?
It seems that NXP should provide the Tresos and its "Activation code" .
but i never found the portal to get the activation code . So i applied the EB Treosos studio package from EB directly :smileyhappy:
So if you find non-evaluative activation code from NXP, please let me know! :smileyhappy:
i stopped the project development on top of ARCCORE for it was bought Vector. ARCCORE would not create the new case, but only support the old projects. i tried to connect to the Vector for the further cooperation two monthes ago, the feedback is "the ARCCORE Would be abandoned ASAP, please just move to the Vector solution " . i think you should pay attention to this change .
congratulations!
two more questions :
1> where did you get the license of the EB tresos ? it took me along time to apply for the evaluation release from EB :smileysad:
2>which kind of the CAN PROBE you are using ?
Hello,
1> When you click on the link below for Elektrobit Tresos Studio / Autosar Configuration Tool, you will see the download links and licence code on the page :smileyhappy: but don't forget toı download the SW by their download tool. In other case, the setup does not work.
I installed Tresos and MCAL setup on my PC today. Tried to change MCAL configuration and wanted to regenerate new MCAL. But didn't work.
I think,there is one more step to do it. Maybe IAR Compiler. not sure. Do you know?
I would be very appreciated if you could help me. The only person who works with the same HW/SW is you :smileyhappy:
2> Vector VN1610. I am working at a passenger/commercial vehicle production company in Turkey. We have lots of that CAN tools :smileyhappy:
Sadan
Hi :
i tried to regenerate the MCAL and got below error messages.
what's you problem ?
0:17:52 **** Build of configuration Default for project HelloWorld_S32K14X ****
make cleantresosgen generateMCAL
==========[ /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X ]===========
SELECT_OPT=OPT_DEBUG file
from rules.mk, /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100
/Rte/Config /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/Contract /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/Config /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/MemMap /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100/core/arch/arm/armv7_m/drivers_stm32/STM32_ETH_Driver /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100/core/arch/arm/armv7_m/drivers_stm32/STM32F10x_StdPeriph_Driver /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/AppSw/Tricore/Cfg_Ssw /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/StartUp_39A/Tricore /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/Compilers/Tricore /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/_Impl /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Scu/Std /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Pms/Std /c/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/ArcticCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Cpu/Std
make[1]: Entering directory `/C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
rm -f -r /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/output/generated
cmd //c /c/devtools/EB/tresos21/bin/tresos_cmd.bat -Dtarget=ARM -Dderivate=S32K14X -data /c/devtools/EB/tresos21/workspace legacy generate -u /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/exports/HelloWorld_MCAL.ARXML@asc:4.2.2 -o /C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/output/generated
EB tresos Studio 21.0.0 b160607-0933
Copyright 2003-2016 Elektrobit Automotive GmbH
INFO 18-09-17,10:18:05 (2102) Reading file "c:\Users\nufront\Desktop\s32k\S32K_StarterKit_2_0_1\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\exports\HelloWorld_MCAL.ARXML"
ERROR 18-09-17,10:18:05 (2094) Cannot find MODULE-DEF refered to by "ContainerDataNode(NAME=MODULE-CONFIGURATION, TYPE=MODULE-CONFIGURATION, VALUE=, XPath=/AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio)"
Errors "1" Warnings "0"
make[1]: *** [generateMCAL] Error 1
make[1]: Leaving directory `/C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
make: *** [/C/Users/nufront/Desktop/s32k/S32K_StarterKit_2_0_1/HelloWorld_S32K14X/HelloWorld_S32K14X] Error 2
10:18:06 Build Finished (took 14s.3ms)
Hello,
After a few email from ARccore support, i havve installed all softwares (ArcticStudio, Arccore, EB, IAR) under the same folder: C:\devtools.
Then i managed to execute “clean s32k144evb_0100”, then “all s32k144evb_0100 GCC” commands (Building HelloWorld_S32K14x steps)
After debugging successfully, i tried the steps given in ADD/CHANGE MCAL CONFIGURATION section.
I opened BSW Editor by clicking on HelloWorld_s32k144evb_Configuration.arxml. Please note that in BSW Editor, “CAN” is not selected and “Can Loop Back Mode” seems as FALSE. But according to Arccore HelloWorld GettingStarted_2.0.1.pdf, it must be TRUE. Can you please check your side? Is it FALSE or TRUE?
I have tried to change “Can Loop Back Mode”from FALSE to TRUE. And clicked on ”regenerate_MCAL”.
Here is the log.
17:10:51 **** Build of configuration Default for project HelloWorld_S32K14X ****
make cleantresosgen generateMCAL
==========[ /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X ]===========
SELECT_OPT=OPT_DEBUG file
from rules.mk, /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100
/Rte/Config /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/Contract /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/Config /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/config/stm32_stm3210c/Rte/MemMap /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100/core/arch/arm/armv7_m/drivers_stm32/STM32_ETH_Driver /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100/core/arch/arm/armv7_m/drivers_stm32/STM32F10x_StdPeriph_Driver /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/AppSw/Tricore/Cfg_Ssw /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/StartUp_39A/Tricore /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/Compilers/Tricore /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/_Impl /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Scu/Std /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Pms/Std /c/devtools/ArcCore/core/system/Os/osal/tricore/aurix/TC39x_Source/IFX_base_famework/BaseFramework_TC39xA/0_Src/BaseSw/iLLD_39A/Tricore/Cpu/Std
make[1]: Entering directory `/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
rm -f -r /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/output/generated
cmd //c /c/devtools/EB/tresos/bin/tresos_cmd.bat -Dtarget=ARM -Dderivate=S32K14X -data /c/devtools/EB/tresos/workspace legacy generate -u /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/exports/HelloWorld_MCAL.ARXML@asc:4.2.2 -o /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/../../MCAL_S32K14X/output/generated
EB tresos Studio 21.0.0 b160607-0933
Copyright 2003-2016 Elektrobit Automotive GmbH
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USDio_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDio_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USDio_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDio_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USDio_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDio_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USEcuM_TS_T40D2M10I1" instead of "EB_TS_MOD_USEcuM_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USEcuM_TS_T40D2M10I1" instead of "EB_TS_MOD_USEcuM_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USEcuM_TS_T40D2M10I1" instead of "EB_TS_MOD_USEcuM_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USWdg_TS_T40D2M10I1R" instead of "EB_TS_MOD_USWdg_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USWdg_TS_T40D2M10I1R" instead of "EB_TS_MOD_USWdg_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:12 (12145) Using a shortened feature name ("EB_TS_MOD_USWdg_TS_T40D2M10I1R" instead of "EB_TS_MOD_USWdg_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USSpi_TS_T40D2M10I1R" instead of "EB_TS_MOD_USSpi_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USSpi_TS_T40D2M10I1R" instead of "EB_TS_MOD_USSpi_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USSpi_TS_T40D2M10I1R" instead of "EB_TS_MOD_USSpi_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USPwm_TS_T40D2M10I1R" instead of "EB_TS_MOD_USPwm_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USPwm_TS_T40D2M10I1R" instead of "EB_TS_MOD_USPwm_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:13 (12145) Using a shortened feature name ("EB_TS_MOD_USPwm_TS_T40D2M10I1R" instead of "EB_TS_MOD_USPwm_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USMcl_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcl_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USMcl_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcl_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USMcl_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcl_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USResource_TS_T40D2M" instead of "EB_TS_MOD_USResource_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USResource_TS_T40D2M" instead of "EB_TS_MOD_USResource_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USResource_TS_T40D2M" instead of "EB_TS_MOD_USResource_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USBase_TS_T40D2M10I1" instead of "EB_TS_MOD_USBase_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USBase_TS_T40D2M10I1" instead of "EB_TS_MOD_USBase_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USBase_TS_T40D2M10I1" instead of "EB_TS_MOD_USBase_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USGpt_TS_T40D2M10I1R" instead of "EB_TS_MOD_USGpt_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USGpt_TS_T40D2M10I1R" instead of "EB_TS_MOD_USGpt_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USGpt_TS_T40D2M10I1R" instead of "EB_TS_MOD_USGpt_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USPort_TS_T40D2M10I1" instead of "EB_TS_MOD_USPort_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USPort_TS_T40D2M10I1" instead of "EB_TS_MOD_USPort_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USPort_TS_T40D2M10I1" instead of "EB_TS_MOD_USPort_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USPort_TS_T40D2M10I1" instead of "EB_TS_MOD_USPort_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:14 (12145) Using a shortened feature name ("EB_TS_MOD_USPort_TS_T40D2M10I1" instead of "EB_TS_MOD_USPort_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:15 (12145) Using a shortened feature name ("EB_TS_MOD_USAdc_TS_T40D2M10I1R" instead of "EB_TS_MOD_USAdc_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:15 (12145) Using a shortened feature name ("EB_TS_MOD_USAdc_TS_T40D2M10I1R" instead of "EB_TS_MOD_USAdc_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:15 (12145) Using a shortened feature name ("EB_TS_MOD_USAdc_TS_T40D2M10I1R" instead of "EB_TS_MOD_USAdc_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USCan_TS_T40D2M10I1R" instead of "EB_TS_MOD_USCan_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USCan_TS_T40D2M10I1R" instead of "EB_TS_MOD_USCan_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USCan_TS_T40D2M10I1R" instead of "EB_TS_MOD_USCan_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USMcu_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcu_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USMcu_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcu_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USMcu_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcu_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:16 (12145) Using a shortened feature name ("EB_TS_MOD_USMcu_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcu_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USMcu_TS_T40D2M10I1R" instead of "EB_TS_MOD_USMcu_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USDem_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDem_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USDem_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDem_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USDem_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDem_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USDem_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDem_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:17 (12145) Using a shortened feature name ("EB_TS_MOD_USDem_TS_T40D2M10I1R" instead of "EB_TS_MOD_USDem_TS_T40D2M10I1R0") for license check.
INFO 18-09-25,17:12:04 (2102) Reading file "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\exports\HelloWorld_MCAL.ARXML"
WARNING 18-09-25,17:12:06 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:06 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1055) Removed node "EcuMEnableDefBehaviour": The schema does not define a parameter with name "EcuMEnableDefBehaviour" in container "ASPath:/TS_T40D2M10I1R0/EcuM/EcuMGeneral".
WARNING 18-09-25,17:12:07 (1055) Removed node "EcuMIncludeDem": The schema does not define a parameter with name "EcuMIncludeDem" in container "ASPath:/TS_T40D2M10I1R0/EcuM/EcuMGeneral".
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/EcuM/ELEMENTS/EcuM/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/EcuM/ELEMENTS/EcuM/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Wdg/ELEMENTS/Wdg/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Wdg/ELEMENTS/Wdg/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Wdg/ELEMENTS/Wdg/WdgSettingsConfig/WdgSettingsConfig_0/WdgInterruptContentEnable" in container "/Wdg/Wdg/WdgSettingsConfig_0"
WARNING 18-09-25,17:12:07 (1055) Removed node "SpiForceDataType": The schema does not define a parameter with name "SpiForceDataType" in container "ASPath:/TS_T40D2M10I1R0/Spi/SpiNonAUTOSAR".
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Spi/ELEMENTS/Spi/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Spi/ELEMENTS/Spi/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1055) Removed node "PwmClockRef": The schema does not define a parameter with name "PwmClockRef" in container "ASPath:/TS_T40D2M10I1R0/Pwm/PwmChannelConfigSet/PwmFtmModule".
WARNING 18-09-25,17:12:07 (1055) Removed node "PwmDiableTrigger": The schema does not define a parameter with name "PwmDiableTrigger" in container "ASPath:/TS_T40D2M10I1R0/Pwm/PwmConfigurationOfOptApiServices".
WARNING 18-09-25,17:12:07 (1055) Removed node "PwmDevErorDetect": The schema does not define a parameter with name "PwmDevErorDetect" in container "ASPath:/TS_T40D2M10I1R0/Pwm/PwmGeneral".
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmChannel/PwmChannel_0/PwmMcuClockReferencePoint" in container "/Pwm/Pwm/PwmChannelConfigSet_0/PwmChannel_0"
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmFtmModule/PwmFtmModule_0/PwmUpdatedEndPeriod" in container "/Pwm/Pwm/PwmChannelConfigSet_0/PwmFtmModule_0"
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmFtmModule/PwmFtmModule_0/PwmUpdatedMiddlePeriod" in container "/Pwm/Pwm/PwmChannelConfigSet_0/PwmFtmModule_0"
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmFtmModule/PwmFtmModule_0/PwmReloadFrequency" in container "/Pwm/Pwm/PwmChannelConfigSet_0/PwmFtmModule_0"
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmConfigurationOfOptApiServices/PwmDisableTrigger" in container "/Pwm/Pwm/PwmConfigurationOfOptApiServices"
WARNING 18-09-25,17:12:07 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmGeneral/PwmDevErrorDetect" in container "/Pwm/Pwm/PwmGeneral"
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Mcl/ELEMENTS/Mcl/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Mcl/ELEMENTS/Mcl/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Resource/ELEMENTS/Resource/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Resource/ELEMENTS/Resource/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Base/ELEMENTS/Base/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Base/ELEMENTS/Base/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1648) Created required node "/Gpt/Gpt/GptPredefTimerConfiguration" in container "/Gpt/Gpt"
WARNING 18-09-25,17:12:08 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptConfigurationOfOptApiServices/GptPredefTimerFunctionalityApi" in container "/Gpt/Gpt/GptConfigurationOfOptApiServices"
WARNING 18-09-25,17:12:08 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptDriverConfiguration/GptPredefTimer100us32bitEnable" in container "/Gpt/Gpt/GptDriverConfiguration"
WARNING 18-09-25,17:12:08 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptDriverConfiguration/GptPredefTimer1usEnablingGrade" in container "/Gpt/Gpt/GptDriverConfiguration"
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Port/ELEMENTS/Port/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Port/ELEMENTS/Port/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:08 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Port/ELEMENTS/Port/PortGeneral/PortSet2PinsDirectionApi" in container "/Port/Port/PortGeneral"
WARNING 18-09-25,17:12:09 (1055) Removed node "AdcHwTrigSrc": The schema does not define a parameter with name "AdcHwTrigSrc" in container "ASPath:/TS_T40D2M10I1R0/Adc/AdcConfigSet/AdcHwUnit/AdcGroup".
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/AdcPublishedInformation/AdcChannelValueSigned to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/AdcPublishedInformation/AdcGroupFirstChannelFixed to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/AdcConfigSet/AdcHwUnit/AdcHwUnit_0/AdcGroup/AdcGroup_0/AdcEnableHalfInterrupt" in container "/Adc/Adc/AdcConfigSet_0/AdcHwUnit_0/AdcGroup_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/AdcConfigSet/AdcHwUnit/AdcHwUnit_0/AdcGroup/AdcGroup_0/AdcPdbPeriodContinuousMode" in container "/Adc/Adc/AdcConfigSet_0/AdcHwUnit_0/AdcGroup_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/CommonPublishedInformation/VendorApiInfix" in container "/Adc/Adc/CommonPublishedInformation"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/NonAutosar/DoubleBufferingMoreThanOneChannel" in container "/Adc/Adc/NonAutosar"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/NonAutosar/AdcEnableDmaTrasferMode" in container "/Adc/Adc/NonAutosar"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/NonAutosar/AdcUseHardwareNormalGroups" in container "/Adc/Adc/NonAutosar"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/NonAutosar/AdcContinuousWithoutInterrupt" in container "/Adc/Adc/NonAutosar"
WARNING 18-09-25,17:12:09 (1055) Removed node "CanFilterMask_0": The schema does not define a parameter with name "CanFilterMask" in container "ASPath:/TS_T40D2M10I1R0/Can/CanConfigSet/CanController".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanIdValue": The schema does not define a parameter with name "CanIdValue" in container "ASPath:/TS_T40D2M10I1R0/Can/CanConfigSet/CanHardwareObject".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanFilterMaskRef": The schema does not define a parameter with name "CanFilterMaskRef" in container "ASPath:/TS_T40D2M10I1R0/Can/CanConfigSet/CanHardwareObject".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanIdValue": The schema does not define a parameter with name "CanIdValue" in container "ASPath:/TS_T40D2M10I1R0/Can/CanConfigSet/CanHardwareObject".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanFilterMaskRef": The schema does not define a parameter with name "CanFilterMaskRef" in container "ASPath:/TS_T40D2M10I1R0/Can/CanConfigSet/CanHardwareObject".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanHardwareCancellation": The schema does not define a parameter with name "CanHardwareCancellation" in container "ASPath:/TS_T40D2M10I1R0/Can/CanGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanIdenticalIdCancellation": The schema does not define a parameter with name "CanIdenticalIdCancellation" in container "ASPath:/TS_T40D2M10I1R0/Can/CanGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "CanCounterRef": The schema does not define a parameter with name "CanCounterRef" in container "ASPath:/TS_T40D2M10I1R0/Can/CanGeneral".
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanControllerIcomSupported" in container "/Can/Can/CanConfigSet_0/CanController_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanWakeupFunctionalityAPI" in container "/Can/Can/CanConfigSet_0/CanController_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanWakeUpSourceFilter" in container "/Can/Can/CanConfigSet_0/CanController_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanHardwareObject/CanHardwareObject_0/CanHwObjectCount" in container "/Can/Can/CanConfigSet_0/CanHardwareObject_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanHardwareObject/CanHardwareObject_1/CanHwObjectCount" in container "/Can/Can/CanConfigSet_0/CanHardwareObject_1"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanGeneral/CanMaxMessageBuffers" in container "/Can/Can/CanGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanGeneral/CanPublicIcomSupport" in container "/Can/Can/CanGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanGeneral/CanMainFunctionRWPeriods/CanMainFunctionRWPeriods_0/CanMainFunctionPeriod" in container "/Can/Can/CanGeneral/CanMainFunctionRWPeriods_0"
WARNING 18-09-25,17:12:09 (1072) Removed "VariableDataNode(NAME=McuRMII_ClkSelect, TYPE=ENUMERATION, VALUE=FIRCDIV1_CLK, XPath=/__internalSubstituteRoot__/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuSIMConfig/McuFlexTimerConfiguration/McuRMII_ClkSelect)" from "/TS_T40D2M10I1R0/Mcu/McuModuleConfiguration/McuSIMConfig/McuFlexTimerConfiguration/McuRMII_ClkSelect": Expected a node of type VariableDataNode(BOOLEAN)
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuPublishedInformation/McuResetReasonConf/MCU_SOFTWARE_RESET/McuResetReason to 2 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuDebugConfiguration/McuDisableCmuApi" in container "/Mcu/Mcu/McuDebugConfiguration"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuDebugConfiguration/McuEnablePeripheralCMU" in container "/Mcu/Mcu/McuDebugConfiguration"
WARNING 18-09-25,17:12:09 (1648) Created required node "/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0/McuClkMonitor_0" in container "/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0/McuClkMonitor_1" in container "/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuClockSettingConfig/McuClockSettingConfig_0/McuSIMClockConfig/McuGPIOClockGatingEnable" in container "/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0/McuSIMClockConfig"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuResetConfig/McuSystemInterruptEnable/McuCMULossOfClockResetInterrupt" in container "/Mcu/Mcu/McuModuleConfiguration_0/McuResetConfig/McuSystemInterruptEnable"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuSIMConfig/McuFlexTimerConfiguration/McuRMII_ClkSelect" in container "/Mcu/Mcu/McuModuleConfiguration_0/McuSIMConfig/McuFlexTimerConfiguration"
WARNING 18-09-25,17:12:09 (1055) Removed node "DemDTCClass_0": The schema does not define a parameter with name "DemDTCClass" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemConfigSet".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemMaxNumberFreezeFrameRecords": The schema does not define a parameter with name "DemMaxNumberFreezeFrameRecords" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemConfigSet/DemEventParameter".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemFreezeFrameRecNumClassRef": The schema does not define a parameter with name "DemFreezeFrameRecNumClassRef" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemConfigSet/DemEventParameter".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemEventClass": The schema does not define a parameter with name "DemEventClass" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemConfigSet/DemEventParameter".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemDTCSuppressionSupport": The schema does not define a parameter with name "DemDTCSuppressionSupport" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemEnableConditionSupport": The schema does not define a parameter with name "DemEnableConditionSupport" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemEventDisplacementSupport": The schema does not define a parameter with name "DemEventDisplacementSupport" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemMaxNumberEventEntryMirror": The schema does not define a parameter with name "DemMaxNumberEventEntryMirror" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemMaxNumberEventEntryPrimary": The schema does not define a parameter with name "DemMaxNumberEventEntryPrimary" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemMaxNumberEventEntrySecondary": The schema does not define a parameter with name "DemMaxNumberEventEntrySecondary" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1072) Removed "VariableDataNode(NAME=DemOBDSupport, TYPE=BOOLEAN, VALUE=0, XPath=/__internalSubstituteRoot__/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemOBDSupport)" from "/TS_T40D2M10I1R0/Dem/DemGeneral/DemOBDSupport": Expected a node of type VariableDataNode(ENUMERATION)
WARNING 18-09-25,17:12:09 (1055) Removed node "DemOperationCycleProcessing": The schema does not define a parameter with name "DemOperationCycleProcessing" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemStorageConditionSupport": The schema does not define a parameter with name "DemStorageConditionSupport" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral".
WARNING 18-09-25,17:12:09 (1055) Removed node "DemFreezeFrameRecordNumber": The schema does not define a parameter with name "DemFreezeFrameRecordNumber" in container "ASPath:/TS_T40D2M10I1R0/Dem/DemGeneral/DemFreezeFrameRecNumClass".
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/CommonPublishedInformation/ArReleaseMinorVersion to 0 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1134) Cannot set the value of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/CommonPublishedInformation/ArReleaseRevisionVersion to 3 because it is readonly. Its DEFAULT is used instead.
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemEventAvailable" in container "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemEventFailureCycleCounterThreshold" in container "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemFFPrestorageSupported" in container "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemOperationCycleRef" in container "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout"
WARNING 18-09-25,17:12:09 (1648) Created required node "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout/DemDebounceAlgorithmClass" in container "/Dem/Dem/DemConfigSet_0/DemEventParameter_ADC_E_Timeout"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemAgingRequieresTestedCycle" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemAvailabilitySupport" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemClearDTCLimitation" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemDataElementDefaultEndianness" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemEventDisplacementStrategy" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemEventMemoryEntryStorageTrigger" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemGeneralInterfaceSupport" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemOBDSupport" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemResetConfirmedBitOnOverflow" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemSuppressionSupport" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/Dem/Dem/DemGeneral/DemPrimaryMemory" in container "/Dem/Dem/DemGeneral"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemOperationCycle/DemOperationCycle_0/DemOperationCycleAutomaticEnd" in container "/Dem/Dem/DemGeneral/DemOperationCycle_0"
WARNING 18-09-25,17:12:09 (1648) Created required node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemOperationCycle/DemOperationCycle_0/DemOperationCycleAutostart" in container "/Dem/Dem/DemGeneral/DemOperationCycle_0"
INFO 18-09-25,17:12:10 (2064) Verify module "EcuM"
WARNING 18-09-25,17:12:10 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/EcuM/ELEMENTS/EcuM/EcuMConfiguration/EcuMCommonConfiguration/EcuMDefaultAppMode" with value "" does not refer to nodes.
WARNING 18-09-25,17:12:10 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/EcuM/ELEMENTS/EcuM/EcuMConfiguration/EcuMCommonConfiguration/EcuMOSResource/__1" with value "" does not refer to nodes.
WARNING 18-09-25,17:12:10 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/EcuM/ELEMENTS/EcuM/EcuMConfiguration/EcuMCommonConfiguration/EcuMSleepMode/EcuMSleepMode_0/EcuMSleepModeMcuModeRef" with value "ASPath:/Mcu/Mcu/McuModuleConfiguration_0/McuModeSettingConf_0" does not refer to nodes.
INFO 18-09-25,17:12:10 (2064) Verify module "Pwm"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmChannel/PwmChannel_0/PwmMcuClockReferencePoint": Invalid or empty reference.
WARNING 18-09-25,17:12:10 (1021) Warning for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmFtmModule/PwmFtmModule_0/PwmFtmChannels/PwmFtmChannels_0/ChannelCombDeadTimeEn": Deadtime insertion should be only used with PHASE_SHIFTED_COMPLEMENTARY or COMBINED_COMPLEMENTARY channel edge setup. If COMBINED_SYNCED/PHASE_SHIFTED_SYNCED is selected and deadtime insertion is used then the odd channel related to COMBINED_SYNCED/PHASE_SHIFTED_SYNCED channel may not work
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmChannelConfigSet/PwmFtmModule/PwmFtmModule_0/PwmFtmChannels/PwmFtmChannels_0/PwmFtmChannelId": please eneble this channel in PwmGeneral/PwmHwConfiguration/PwmChannelIsUsed
ERROR 18-09-25,17:12:10 (1065) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Pwm/ELEMENTS/Pwm/PwmGeneral/PwmHwConfiguration" has not enough children! It has "0" child - allowed are "40" to "40" children. The children are: []
INFO 18-09-25,17:12:10 (2064) Verify module "Gpt"
ERROR 18-09-25,17:12:10 (1065) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptHwConfiguration" has not enough children! It has "0" child - allowed are "22" to "22" children. The children are: []
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptFtmPrescaler": Value out of range: is "0" but must be "> 0" and "< 129"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptFtmPrescaler_Alternate": Value out of range: is "0" but must be "> 0" and "< 129"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptHwChannel": This channel has not been configured for use yet. Please refer to GptHwConfiguration to configure!
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptHwChannel": If continuous mode is used for current channel then its ISRs shall be enabled for current timer module.
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptLptmrPrescaler": Value out of range: is "0" but must be "> 0" and "< 65537"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_LedBlinker/GptLptmrPrescaler_Alternate": Value out of range: is "0" but must be "> 0" and "< 65537"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptFtmPrescaler": Value out of range: is "0" but must be "> 0" and "< 129"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptFtmPrescaler_Alternate": Value out of range: is "0" but must be "> 0" and "< 129"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptHwChannel": This channel has not been configured for use yet. Please refer to GptHwConfiguration to configure!
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptHwChannel": If continuous mode is used for current channel then its ISRs shall be enabled for current timer module.
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptLptmrPrescaler": Value out of range: is "0" but must be "> 0" and "< 65537"
ERROR 18-09-25,17:12:10 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Gpt/ELEMENTS/Gpt/GptChannelConfigSet/GptChannelConfiguration/GptChannelConfiguration_WdgTrig/GptLptmrPrescaler_Alternate": Value out of range: is "0" but must be "> 0" and "< 65537"
INFO 18-09-25,17:12:11 (2064) Verify module "Adc"
ERROR 18-09-25,17:12:11 (1065) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Adc/ELEMENTS/Adc/AdcInterrupt" has not enough children! It has "0" child - allowed are "2" to "*" children. The children are: []
INFO 18-09-25,17:12:11 (2064) Verify module "Can"
ERROR 18-09-25,17:12:11 (1025) Value "Polling" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanBusoffProcessing" not in range "[INTERRUPT, POLLING]"
ERROR 18-09-25,17:12:11 (1025) Value "Polling" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanRxProcessing" not in range "[INTERRUPT, POLLING]"
ERROR 18-09-25,17:12:11 (1025) Value "Polling" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanTxProcessing" not in range "[INTERRUPT, POLLING]"
ERROR 18-09-25,17:12:11 (1025) Value "Polling" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanWakeupProcessing" not in range "[INTERRUPT, POLLING]"
WARNING 18-09-25,17:12:11 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanCpuClockRef_Alternate" with value "ASPath:/Mcu/Mcu/McuModuleConfiguration_0/McuClockSettingConfig_0/McuClockReferencePoint_0" does not refer to nodes.
WARNING 18-09-25,17:12:11 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanConfigSet/CanController/CanController_0/CanWakeupSourceRef" with value "" does not refer to nodes.
WARNING 18-09-25,17:12:11 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Can/ELEMENTS/Can/CanGeneral/CanSupportTTCANRef" with value "" does not refer to nodes.
INFO 18-09-25,17:12:12 (2064) Verify module "Mcu"
ERROR 18-09-25,17:12:11 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuGeneralConfiguration/McuEnterLowPowerMode": The McuAllowVeryLowPowerModes and McuEnterLowPowerMode must be same configuration (true or false)
ERROR 18-09-25,17:12:11 (1032) Value "1" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuClockSettingConfig/McuClockSettingConfig_0/McuClockSettingId" is out of range: For input string: "Value out of range: must be in range 0 to N-1 (N is number of configured clock setting). Use the Calculate button to calculate correct default value."
ERROR 18-09-25,17:12:12 (1032) Value "3" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuModuleConfiguration/McuModeSettingConf/McuModeSettingConf_SLEEP/McuMode" is out of range: For input string: "Value out of range: must be in range 0 to N-1 (N is number of configured Mode setting). Use the Calculate button to calculate correct default value."
ERROR 18-09-25,17:12:12 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Mcu/ELEMENTS/Mcu/McuPublishedInformation/McuResetReasonConf/MCU_SOFTWARE_RESET/McuResetReason": Value "" is no number
INFO 18-09-25,17:12:12 (2064) Verify module "Dem"
ERROR 18-09-25,17:12:12 (1023) Invalid boolean value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemEventAvailable". Expected either "true" as true or "false" as false
ERROR 18-09-25,17:12:12 (1023) Invalid boolean value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemFFPrestorageSupported". Expected either "true" as true or "false" as false
WARNING 18-09-25,17:12:12 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemOperationCycleRef" with value "" does not refer to nodes.
WARNING 18-09-25,17:12:12 (1069) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemConfigSet/DemEventParameter/DemEventParameter_ADC_E_Timeout/DemDebounceAlgorithmClass/DemDebounceCounterBasedClassRef" with value "" does not refer to nodes.
ERROR 18-09-25,17:12:12 (1023) Invalid boolean value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemAgingRequieresTestedCycle". Expected either "true" as true or "false" as false
ERROR 18-09-25,17:12:12 (1025) Value "" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemAvailabilitySupport" not in range "[DEM_EVENT_AVAILABILITY, DEM_NO_AVAILABILITY]"
ERROR 18-09-25,17:12:12 (1025) Value "" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemDataElementDefaultEndianness" not in range "[BIG_ENDIAN, LITTLE_ENDIAN, OPAQUE]"
ERROR 18-09-25,17:12:12 (1025) Value "" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemEventDisplacementStrategy" not in range "[DEM_DISPLACEMENT_FULL, DEM_DISPLACEMENT_NONE, DEM_DISPLACEMENT_PRIO_OCC]"
ERROR 18-09-25,17:12:12 (1025) Value "DEM_STORAGE_ON_TEST_FAILED" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemEventMemoryEntryStorageTrigger" not in range "[DEM_TRIGGER_ON_CONFIRMED, DEM_TRIGGER_ON_FDC_THRESHOLD, DEM_TRIGGER_ON_PENDING, DEM_TRIGGER_ON_TEST_FAILED]"
ERROR 18-09-25,17:12:12 (1023) Invalid boolean value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemGeneralInterfaceSupport". Expected either "true" as true or "false" as false
ERROR 18-09-25,17:12:12 (1025) Value "" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemOBDSupport" not in range "[DEM_OBD_DEP_SEC_ECU, DEM_OBD_MASTER_ECU, DEM_OBD_NO_OBD_SUPPORT, DEM_OBD_PRIMARY_ECU]"
ERROR 18-09-25,17:12:12 (1025) Value "" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemSuppressionSupport" not in range "[DEM_DTC_SUPPRESSION, DEM_NO_SUPPRESSION]"
ERROR 18-09-25,17:12:12 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemTaskTime": Value out of range: is "0.0" but must be ">= 0.001" and "<= 0.1"
ERROR 18-09-25,17:12:12 (1065) The node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemFreezeFrameRecNumClass/DemFreezeFrameRecNumClass_0/DemFreezeFrameRecordClassRef" has not enough children! It has "0" child - allowed are "1" to "254" children. The children are: []
ERROR 18-09-25,17:12:12 (1019) Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Dem/ELEMENTS/Dem/DemGeneral/DemPrimaryMemory/DemMaxNumberEventEntryPrimary": Value "" is no number
INFO 18-09-25,17:12:12 (2113) Creating directory "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated"
INFO 18-09-25,17:12:12 (13030) Running generator "Dio_TS_T40D2M10I1R0" in mode "generate" for module "Dio_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (2113) Creating directory "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\output"
INFO 18-09-25,17:12:12 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Dio.epc
INFO 18-09-25,17:12:12 (13030) Running generator "Dio_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Dio_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Dio_Cfg.h"
INFO 18-09-25,17:12:12 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Dio_Cfg.c"
INFO 18-09-25,17:12:12 (13030) Running generator "EcuM_TS_T40D2M10I1R0" in mode "generate" for module "EcuM_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\EcuM.epc
INFO 18-09-25,17:12:12 (13030) Running generator "EcuM_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "EcuM_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\EcuM_Cfg.h"
INFO 18-09-25,17:12:12 (13030) Running generator "Wdg_TS_T40D2M10I1R0" in mode "generate" for module "Wdg_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Wdg.epc
INFO 18-09-25,17:12:12 (13030) Running generator "Wdg_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Wdg_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:12 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Wdg_Lcfg.c"
INFO 18-09-25,17:12:12 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Wdg_CfgExt.c"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Wdg_PBcfg.c"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Wdg_Cfg.h"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Wdg_Cfg.c"
INFO 18-09-25,17:12:13 (13030) Running generator "Spi_TS_T40D2M10I1R0" in mode "generate" for module "Spi_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:13 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Spi.epc
INFO 18-09-25,17:12:13 (13030) Running generator "Spi_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Spi_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Spi_PBcfg.c"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Spi_Cfg.h"
INFO 18-09-25,17:12:13 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Spi_Cfg.c"
INFO 18-09-25,17:12:13 (13030) Running generator "Pwm_TS_T40D2M10I1R0" in mode "generate" for module "Pwm_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:13 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Pwm.epc
INFO 18-09-25,17:12:13 (13030) Running generator "Pwm_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Pwm_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:14 (2091) Failed to run generator "Pwm_TS_T40D2M10I1R0_GeneratorId" (mode: "generate") for module "Pwm_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:14 (1806) Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Pwm_TS_T40D2M10I1R0/generate_PB/src/Pwm_PBcfg.c (signed)", line "299"
Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Pwm_TS_T40D2M10I1R0/generate_PB/src/Pwm_PBcfg.c (signed)", line "299"
Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Pwm_TS_T40D2M10I1R0/generate_PB/src/Pwm_PBcfg.c (signed)", line "299"
The XPath-expression "node:ref(PwmMcuClockReferencePoint)/McuClockReferencePointFrequency" caused an error: (1844) No node found for path ""
ERROR 18-09-25,17:12:14 (2070) Failed to generate file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Pwm_TS_T40D2M10I1R0/generate_PB/src/Pwm_PBcfg.c (signed)"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Pwm_Cfg.h"
INFO 18-09-25,17:12:14 (13030) Running generator "Mcl_TS_T40D2M10I1R0" in mode "generate" for module "Mcl_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Mcl.epc
INFO 18-09-25,17:12:14 (13030) Running generator "Mcl_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Mcl_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\CDD_Mcl_Cfg.c"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\CDD_Mcl_PBcfg.c"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\CDD_Mcl_Cfg.h"
INFO 18-09-25,17:12:14 (13030) Running generator "Resource_TS_T40D2M10I1R0" in mode "generate" for module "Resource_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Resource.epc
INFO 18-09-25,17:12:14 (13030) Running generator "Resource_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Resource_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (13030) Running generator "Base_TS_T40D2M10I1R0" in mode "generate" for module "Base_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Base.epc
INFO 18-09-25,17:12:14 (13030) Running generator "Base_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Base_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\modules.h"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Reg_eSys.h"
INFO 18-09-25,17:12:14 (13030) Running generator "Gpt_TS_T40D2M10I1R0" in mode "generate" for module "Gpt_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:14 (2091) Failed to run generator "Gpt_TS_T40D2M10I1R0_GeneratorId" (mode: "generate") for module "Gpt_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:14 (1806) Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Gpt_TS_T40D2M10I1R0/generate_PB/Gpt_PluginMacros.m (signed)", line "396"
Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Gpt_TS_T40D2M10I1R0/generate_PB/Gpt_PluginMacros.m (signed)", line "396"
Parsing file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Gpt_TS_T40D2M10I1R0/generate_PB/Gpt_PluginMacros.m (signed)", line "396"
The XPath-expression "node:ref($path_predef)" caused an error: (1844) No node found for path "GptPredefTimerConfiguration/GptPredefTimer_1us_16Bit"
ERROR 18-09-25,17:12:14 (2070) Failed to generate file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Gpt_TS_T40D2M10I1R0/generate_PB/src/Gpt_PBcfg.c (signed)"
INFO 18-09-25,17:12:14 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Gpt.epc
INFO 18-09-25,17:12:14 (13030) Running generator "Gpt_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Gpt_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Gpt_Cfg.h"
INFO 18-09-25,17:12:14 (13030) Running generator "Port_TS_T40D2M10I1R0" in mode "generate" for module "Port_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:14 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Port.epc
INFO 18-09-25,17:12:14 (13030) Running generator "Port_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Port_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Port_Cfg.c"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Port_PBcfg.c"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Port_Cfg.h"
INFO 18-09-25,17:12:15 (13030) Running generator "Os_TS_T40D2M10I1R0" in mode "generate" for module "Os_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:15 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Os.epc
INFO 18-09-25,17:12:15 (13030) Running generator "Os_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Os_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Os_cfg.h"
INFO 18-09-25,17:12:15 (13030) Running generator "Adc_TS_T40D2M10I1R0" in mode "generate" for module "Adc_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:15 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Adc.epc
INFO 18-09-25,17:12:15 (13030) Running generator "Adc_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Adc_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Adc_CfgDefines.h"
INFO 18-09-25,17:12:15 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Adc_Cfg.c"
INFO 18-09-25,17:12:16 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Adc_PBcfg.c"
INFO 18-09-25,17:12:16 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Adc_Cfg.h"
INFO 18-09-25,17:12:16 (13030) Running generator "Can_TS_T40D2M10I1R0" in mode "generate" for module "Can_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:16 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Can.epc
INFO 18-09-25,17:12:16 (13030) Running generator "Can_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Can_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:16 (2091) Failed to run generator "Can_TS_T40D2M10I1R0_GeneratorId" (mode: "generate") for module "Can_TS_T40D2M10I1R0"
ERROR 18-09-25,17:12:16 (2004) [C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Can_TS_T40D2M10I1R0/generate_PC/include/Can_Cfg.h (signed):218]: The "CanHwFilter" of each HOH must be enabled when user configure HOH is receive.
(node )
ERROR 18-09-25,17:12:16 (2070) Failed to generate file "C:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_P2_1_0_1\eclipse\plugins\Can_TS_T40D2M10I1R0/generate_PC/include/Can_Cfg.h (signed)"
INFO 18-09-25,17:12:16 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Can_PBcfg.c"
INFO 18-09-25,17:12:16 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Can_Cfg.c"
INFO 18-09-25,17:12:16 (13030) Running generator "Mcu_TS_T40D2M10I1R0" in mode "generate" for module "Mcu_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:16 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Mcu.epc
INFO 18-09-25,17:12:16 (13030) Running generator "Mcu_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Mcu_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:17 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Mcu_Cfg.h"
INFO 18-09-25,17:12:17 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Mcu_PBcfg.c"
INFO 18-09-25,17:12:17 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\src\Mcu_Cfg.c"
INFO 18-09-25,17:12:17 (13030) Running generator "Dem_TS_T40D2M10I1R0" in mode "generate" for module "Dem_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:17 (20053) Generating file C:\devtools\MCAL_S32K14X\output\generated\output\Dem.epc
INFO 18-09-25,17:12:17 (13030) Running generator "Dem_TS_T40D2M10I1R0_GeneratorId" in mode "generate" for module "Dem_TS_T40D2M10I1R0"
INFO 18-09-25,17:12:17 (13014) Generated "c:\devtools\HelloWorld_S32K14X\HelloWorld_S32K14X\..\..\MCAL_S32K14X\output\generated\include\Dem_IntErrId.h"
Errors "47" Warnings "122"
make[1]: *** [generateMCAL] Error 1
make[1]: Leaving directory `/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
make: *** [/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X] Error 2
17:12:20 Build Finished (took 1m:28s.942ms)
I have asked this to Arccore Support. They say that the errors are related to Tresos. So they can not give support :smileysad:
This is a roadblock for me. Our Tresos version is 21.0.0 and it is compatible with the mentioned in pdf file.
Sadan
Hello,
Would you mind give me your personal email address? Would be better for communication.
Here is the
Here is what i am doing from the beginning...
1)
I used HelloWorld_S32K14X (green) to get the project running on my board. (Arccore HelloWorld GettingStarted_2.0.1.pdf, RUNNING EXAMPLE ON NXP S32K144EVB-Q100v).
Project Name: Debug_3_HelloWorld_S32k14X.elf (Step 6)
After Step 10, it starts to work on my PC. As i said before, i can see CAN messages. These are all OK.
2)
For ADD/CHANGE MCAL CONFIGURATION, i double click on HelloWorld_S32K144evb_Configuration.arxml. Then HelloWorld - BSW Editor window opens. I just want to change CAN Baud Rate as a simple update.
So, i double click on Can (green). A new window oppens. (Figure 10 in Arccore HelloWorld GettingStarted_2.0.1.pdf)
I tried also to change ”Can Loop Back Mode” parameter. Then i click on "regenerate_MCAL" on the right side.
Here is the result:
09:44:32 **** Build of configuration Default for project HelloWorld_S32K14X ****
make cleantresosgen generateMCAL
gawk: fatal: can't open source file `/c/Program' for reading (No such file or directory)
==========[ /C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X ]===========
make[1]: /c/Program: No such file or directory
make[1]: Entering directory `/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
make[1]: *** No rule to make target `/c/Program'. Stop.
make[1]: Leaving directory `/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X/obj_s32k144evb_0100'
make: *** [/C/devtools/HelloWorld_S32K14X/HelloWorld_S32K14X] Error 2
09:45:06 Build Finished (took 33s.667ms)
It tries to open "/c/Program" but there is no such folder in my PC.
I didn't understand where i am doing wrong.
Sadan
nothing special , but follow the "readme" file named "Arccore HelloWorld GettingStarted_2.0.1.pdf". i encountered some issues as below :
1> you must select the right debugging interface as yellow highlighted
2>select the interface settings correctly and make sure the right port " USB1-OpenSDA(xxxxx) " is found .
3> select the right target device
4>assign the right gdb client
so what's your problems?
Hello guohua wu,
Thank you very much. I couldn't solve installation issues yet. First, i have installed Arctic Studio. I have downloaded AUTOSAR Tresos Studio 21.0.0 from a link from NXP but could not install it. When i i try Setup.exe, it gives error about file papckages. I am trying to find the same link or another to download the SW again.
Do you have the links?
Thanks
Sadan
From S32K14x MCAL package , i found the link below
I have downloaded the MCAL and Tresos Studio.
While trying to setup, it gives "no packages was found..." error.
Hello,
To resolve the issue "No packages were found that can be installed" rename all the files with .gz extension to .uip. Some browsers can change the file extension. Hope this helps.
Hello,
Yes, it worked :smileyhappy: I have installed PEMicro Driver for USB OpenDSA. I checked CAN port and saw ID 0x001 message with 200ms cycle. But the last 4 byte always 0x00. They should display ADC value.
Now, the next step is to play with the code and try to understand how it works. I think, EB Tresos is required now.
Hello guohua wu,
In these days, I am trying to get S32K144 EVB board to run with HelloWorld application like you. But I couldn’t succeed
Can you please help me?
Sadan