I configured a S32K project of CAN communication.but when I run it ,it doesn't work.there is too many parameters in a EB project,I can't configured it correctly without help.is there any document or something to read about it?or is there anywhere that I can download a Demo project that runs well?
Hi GaoWei,
I remember that in your last question you used non-AUTOSAR MCAL routines in S32DS with RTD.
Do you need to use EB tresos to configure CAN routines this time?
There are routines for EB tresos in the latest S32K1 Real-Time Drivers Version 1.0.1 for your reference
After install it, you should be able to import Can_example_S32K144 routine with tresos Studio 27.1.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi dear Robin
I downloaded the RTD and installed it ,and I can open a example project,but when I double click it,I saw this
Did I installed it wrongly?
Hi dear Robin:
I clicked S32K1 Real-Time Drivers Version 1.0.1 and opened the link ,and only saw this:
Do I need to pay for the RTD or buy something to get it?