The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool

跳至解决方案
1,057 次查看
shuo41
Contributor III

The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool,why?bitrate configured by s32dsbitrate configured by s32dscan tool on pc(through can Analyser)can tool on pc(through can Analyser)

0 项奖励
回复
1 解答
919 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

share project which shows the issue so we can check.

BR, Petr

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,041 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check if selected protocol clock is really the one you specified (40MHz) within clock config.

BR, Petr

0 项奖励
回复
1,030 次查看
shuo41
Contributor III

It is 40MHZ 

clock.pngclock2.png

0 项奖励
回复
1,021 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

then check if clock is really configured and system clock running from PLL. Also measure TXD line with scope/analyzer to know real bitrate.

You can also check FlexCAN bit timing registers for values written.

BR, Petr

 

0 项奖励
回复
924 次查看
shuo41
Contributor III

I am testing LIN.When I fill in the baud rate column with 9600, my logic analyzer cannot receive data correctly at 9600.When I fill in the baud rate column with 3700, my logic analyzer correctly receives data at 9600.22.png44.png77.png66.png55.png

0 项奖励
回复
920 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

share project which shows the issue so we can check.

BR, Petr

 

0 项奖励
回复
900 次查看
shuo41
Contributor III

HI,I Solved the problem. My external clock configuration is incorrect.The external clock is 40MHz, and I have configured it to be 16MHz.Thinks for your help.

0 项奖励
回复
926 次查看
shuo41
Contributor III

Its source is PLL, that's right. The bit rate measured by my oscilloscope is incorrect.I test Lin, The baud rate it outputs is also incorrect.11.png

0 项奖励
回复