Segger debug configuration not showing in S32 design studio 2018.R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segger debug configuration not showing in S32 design studio 2018.R1

Jump to solution
8,649 Views
rohit_rawat
Contributor I

Hey All,

I'm not getting any GDB segger jlink configuration in debug configuration in my S32 design studio as like GDB hardware debugging, GDB PEMicro interface debugging etc. but can not get the same for GDB segger jlink.

Thank you.

 

 

0 Kudos
Reply
1 Solution
8,585 Views
jiri_kral
NXP Employee
NXP Employee

This is strange, as far as I know - S32DS for Arm is not supporting S32 Debug probe. Please try to create new workspace and try it again: 

jiri_kral_0-1604404779240.png

 

 

 

View solution in original post

0 Kudos
Reply
9 Replies
8,634 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

When you create a new project, you need to select Segger J-link GBD server as the debugger.

danielmartynek_0-1604323896343.png

 

BR, Daniel

 

 

0 Kudos
Reply
8,628 Views
rohit_rawat
Contributor I

Dear sir,

I did not get any option related to Segger jlink in debbuger while creating new project

I am getting only PE and s32 debugger here. 

Please resolve the issue.

Thank you.

0 Kudos
Reply
8,623 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can check for updates / new SW.

danielmartynek_0-1604394457397.png

But I would recommend using a newer version of the Design Studio.

S32 Design Studio for ARM 2.2 – Windows/Linux

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

S32 Design Studio 3.3 – Windows/Linux

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

 

BR, Daniel

 

0 Kudos
Reply
8,610 Views
rohit_rawat
Contributor I

Dear sir,

I downloaded S32 Design Studio for ARM 2.2 and installed it online. After installing i got segger jlink debugger but this S32ds showing errors "make" not found in PATH, Ld error etc. as shown in fig.

0 Kudos
Reply
8,583 Views
jiri_kral
NXP Employee
NXP Employee

Did you created your project as a S32DS application project? 

jiri_kral_0-1604404887662.png

With this option all paths should be configured correctly for new project. You can check it in project properties: 

jiri_kral_1-1604404981082.png

 

Jiri

 

0 Kudos
Reply
8,599 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

on your screenshot is probably S32DS v3.3 - not S32DS for ARM v2.2. Please make sure that you installed correct S32DS Version. 

 

Jiri

0 Kudos
Reply
8,594 Views
rohit_rawat
Contributor I

Dear  sir,

It is S32 Design Studio for ARM Version: 2.2. Please review the attached image.

Thank you

 

0 Kudos
Reply
8,586 Views
jiri_kral
NXP Employee
NXP Employee

This is strange, as far as I know - S32DS for Arm is not supporting S32 Debug probe. Please try to create new workspace and try it again: 

jiri_kral_0-1604404779240.png

 

 

 

0 Kudos
Reply
8,580 Views
rohit_rawat
Contributor I

Dear sir,

After switching working it works smoothly. Thank you for your initiative.

Thank you sir

0 Kudos
Reply