SPI communication in S32K358 Evboard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI communication in S32K358 Evboard

Jump to solution
571 Views
Changwoo82
Contributor II

Hello!

I'm a hardware developer with a beginner-level understanding of software.
I'd like to perform SPI communication using an Evaluation board that integrates S32K358 and FS26.
Could I get the any reference materials or source code examples I could use?

Thank you.

0 Kudos
Reply
1 Solution
533 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Changwoo82,

There are Automotive SW - SBC/PMIC - Real Time Drivers for S32K3xx.

It is a part of the S32K3 Standard Software

danielmartynek_0-1696931377862.png

 

Refer to the release notes for more information about the driver.

SW32K3_FS26_R21-11_2.0.0_D2308_Release_Notes.pdf

 

Best regards,

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
534 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Changwoo82,

There are Automotive SW - SBC/PMIC - Real Time Drivers for S32K3xx.

It is a part of the S32K3 Standard Software

danielmartynek_0-1696931377862.png

 

Refer to the release notes for more information about the driver.

SW32K3_FS26_R21-11_2.0.0_D2308_Release_Notes.pdf

 

Best regards,

Daniel

0 Kudos
Reply