S32k358 I work on SBC_fs26 and I found this error ('Sbc_fs26_PBCfgVariantPredefined' undeclared (first use in this function)), taking in consideration that we are working using precompile option
I noticed that the value for " -Dcom.nxp.swtools.codegenscript.timeout=60000 " is different . It's currently set to a different value.
Do I need to change this value??
Dear Mariam,
I am not sure, why the " -Dcom.nxp.swtools.codegenscript.timeout=60000 " line appeared in your S32DS.ini file. I have checked my S32DS.ini file and I don't have the line there. Please rewrite the " -Dcom.nxp.swtools.codegenscript.timeout=60000 " with the recommended -"Dcom.nxp.swtools.codegenscript.timeout=-1"
With Best Regards,
Jozef
Dear Mariam,
please see a solution below, where another customer had similar issue.
DESCRIPTION
There can be multiple reasons for the failure, here is a list:
“In case of difficulties in the code generation using S32 Configuration due to computer speed, it is possible to remove the timeout in the C:\NXP\S32DS.3.4\eclipse\s32ds.ini file by adding the following line: -Dcom.nxp.swtools.codegenscript.timeout=-1.”
Or if you are using the S32DS version 3.5, then in C:\NXP\S32DS.3.5\eclipse\s32ds.ini
After adding this in .ini file please restart S32DS and create a new workspace where a fresh import has to be tried.
With Best Regards,
Jozef
Hi Jozef,
Thanks for your support but I have concerns:
1-We are configuring from Tresos tool, not design studio.
2-Also it is noticed that SBC_FS26_CONFIG_EXT define has no replacement parameter in the generated file CDD_Sbc_Fs26_Cfg.h
It is only generated correctly through Design studio
Below screenshot from configuration through Tresos
Following screenshot from configuring through design studio
Note:
SBC package version: S32K3_FS26_R21-11_2.0.0_CD01
Hi Marina,
I have contacted an application team for an advice. So far there is no answer from them. As soon as they answer me, I will definitely reply to you.
Thank you for your patience.
With Best Regards,
Jozef
Hi Marina,
I apologize for a late reply. The application team have informed me, that they are working on the case. As soon as they send me another answer, I will definitely reply to you.
Thank you for your patience.
With Best Regards,
Jozef
Hi Marina,
please see a suggestion from the application team. Please test it.
DESCRIPTION
I think the problem is that the customer did not clicked on the Post Build Variant Used check box.
Can they try this and see if the error is still there?
With Best Regards,
Jozef
Hi Marina,
please see below an answer from the application team.
DESCRIPTION
Please tell the customer to update to the RTM version of the SBC_FS26, SW32K3_FS26_R21-11_2.0.0_D2308, it is compatible with RTD 3.0.0. And configure the SBC as it follows.
This is avaiable in the bundle in package manager S32K358 HVBMS: Automotive Software Package Manager | NXP Semiconductors
With Best Regards,
Jozef
I can't install it !
Hi Mariam,
are you able to generate the Bundle Installer? Please share a printscreen view, of the Package Manager. How you see it on your side.
With Best Regards,
Jozef
Hi Mariam,
thank you for the update. Could you please confirm the software and hardware you are using?
Please state the full Evaluation Board number you are using. Is it RD-K358BMU or RD-K344BMU, or any other? Or are you working on your own board?
Which S32DS IDE you are using? 3.4 or 3.5?
With Best Regards,
Jozef
using S32k3X8EVB-Q289 "SCH-89070 REV A3"
Design studio version 3.5
Hi Mariam,
thank you very much for confirmation. This clears out, why you cannot download the recommended software. It seems you do not have a license for it. The license comes with HVBMS EVBs. So you are not using our RD-K358BMU EVB for HVBMS. This is question for different application team. I have contacted the other team. As soon as they answer me, I will definitely reply to you.
Thank you for your patience.
With Best Regards,
Jozef
Hi Mariam,
the application team suggests to use S32K3 FS26 RTM version. I have download it for you. Please find it attached.
DESCRIPTION
I see the issue was reported on version 2.0.0 CD01
Can you please suggest they try 2.0.0 RTM instead?
With Best Regards,
Jozef
the issue still exist
Hi Mariam,
do you receive the same error ('Sbc_fs26_PBCfgVariantPredefined' undeclared (first use in this function)) with the S32K3 FS26 RTM version software? Or is there an other error message?
With Best Regards,
Jozef