When I am reading the datasheet about BCTU, I am very confused about the descripition of BCTU interrupt .
my application:
BCTU trigger 4 ADC sample, ADC0_ch1,ADC1_ch1,ADC2_ch1,ADC2_ch2.
conversion of ADC0_ch1,ADC1_ch1,ADC2_ch1 started simultaneous,then ADC2_ch2 start conversion.
And I don't use DMA to transfer ADC data.
the following come from attachment of the datasheet(.xlsx).
the following come from the datasheet.
If I configure "Event" as "CL Last"(MCR[LIST_IEN]=1), sampleing of the ADC2_ch2 just started, not finished?
I just want to find a interrupt that interrupt request when all sample of CL list finished.
解決済! 解決策の投稿を見る。
Hi,
ideally it would be to use different ADC in normal mode for slow tasks, I think.
BR, Petr
Hi,
this description indicates, the interrupt is triggered when ADC command is issued, not ADC conversion completed. However MCR[LIST_IEN] and MSR[LISTn_Last] description shows little bit different meaning.
Let me check that with Apps/design team.
Anyway is your case it would be better to put results into FIFO and generate interrupt on FIFO watermark. Set FIFO watermark=3 and interrupt will be called once 4 results will be placed there, means all conversions from a list.
BR, Petr
Maybe FIFO have its limit.
if I set FIFO watermark=2,I sample 3current and 7 other signal.
FIFO interrupt would happen 3 times? one interrupt for 3 signal, 3 interrupt for 9 signal.
Hi,
yes, it can work this way.
If you read 3 results from FIFO within interrupt, then this interrupt will be called 2 times within PWM period if 8 results are stored. In 2nd interrupt call you can read rest of result as should be finished already. FIFOCNTR indicates active entries in FIFO.
BR, Petr
Hi,
ideally it would be to use different ADC in normal mode for slow tasks, I think.
BR, Petr
This is important for our hardware design of controlboard, So I need to double check the usage.
PWM enable Half-period load and full period load. PWM period is 100us, so the interrupt is 50us.
PWM trigger -> TRGMUX -> BCTU0 -> ADC -> BCTU0_FIFO_FOC interrupt.
CL list configured in BCTU0:
ADC0_1 for currentU
ADC1_1 for currentV
ADC2_1 for currentW
ADC0_2 for Udc
ADC1_2 for U_KL15
ADC2_2 for U_KL30
ADC0_3 for U_Tmotor1(NTC)
ADC1_3 for U_Tmotor2(NTC)
Use FIFO in BCTU, set watermark=2.
timeline:
T0: PWM trigger generated, and trigger transfer to BCTU by TRGMUX.
T1(4~5 BCTU clock after T0): BCTU trigger ADC sample.
T2(about 1us after T1,conversion time is about 1us): currentUVW sample finished; Udc sample not finished; FOC calculation started.
T3(about 30-40us(FOC calculation time) after T2): FOC calculation finished; read ADC result of Udc,KL15,KL30,Tmotor1,Tmotor2.
In this way, I don't need to waste time waiting for other ADC(Udc,KL15,KL30,Tmotor1,Tmotor2) conversion in interrupt task, and I still get what I want.
Can that work?