S32K312 Standby Current Consumption

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K312 Standby Current Consumption

跳至解决方案
4,199 次查看
kjy106906
Contributor IV

Currently I am testing with the S32K312EVB-Q172.
The datasheet shows that the standby current consumption of S32K312 is about 50uA based on VDD 5V.
However, when measuring the current consumption of MCU VDD with EVB, it comes out to about 350uA. (based on VDD 5V)
When VDD is 3V, it measures about 80uA.
Can you tell me why EVB's standby current consumption is different from DataSheet?

0 项奖励
回复
1 解答
4,103 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, a typo, I just edited it, sorry for that.

Let me check.

The project tested is attached.

 

BR, Daniel

在原帖中查看解决方案

16 回复数
4,194 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

Where do you measure the consumption?

Did you removed R303 and R349 and do you measure if at J10, J15?

danielmartynek_0-1658407208110.png

 

BR, Daniel

0 项奖励
回复
4,192 次查看
kjy106906
Contributor IV

Hello @danielmartynek 

Thanks for the reply
My question is about the S32K312EVB-Q172.
There seems to be no J15 here.

I removed R303 and measured the current at J10.

What is the standby current consumption of your board?

0 项奖励
回复
4,190 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

You are right, only J10 (VDD_HV_A_MCU) on S32K312.

I don't have the board right now to test it.

But anyway, it depends on what is running on that MCU.

Table 14 specifies the power consumption at certain conditions specified in Table 20.

Also, it does not include any external load on the pins.

Please use the S32K Power Estimation Tool to estimate the consumption.

danielmartynek_0-1658413033938.png

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-general-pu...

For example, if FIRC is enabled in the Standby mode, the power consumption increases to 887uA.

danielmartynek_1-1658413151907.png

 

Regards,

Daniel

0 项奖励
回复
4,174 次查看
kjy106906
Contributor IV

Thank you for the reply @danielmartynek 
I don't use FIRC in Standby mode.
And MCU VDD consumption current is also strange at 350uA.
Can you measure the STANDBY mode current consumption of the S32K144?
(Or ask another team)

0 项奖励
回复
4,154 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

I got the S32K312 EVB and tested it with a similar result.

Let me look into it.

 

BR, Daniel

 

 

0 项奖励
回复
4,149 次查看
kjy106906
Contributor IV

Thanks for the test @danielmartynek 
I will wait for your results

Best Regards

Junyeong Kim

0 项奖励
回复
4,109 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

I could not lower the consumption on the S32K312 EVB.

So I asked a colleague of mine to test same code on this EVB and another NXP internal board that I don't have.

On the S32K312 EVB, HV_A = 5V, current at J10 = ~350uA.

On the internal board, HV_A = 5V, HV_A current = 42.56uA.

Not sure what is the root cause here, but it seems to be an issue of the EVB not the MCU.

You should get lower consumption when testing on your custom board.

 

Regards,

Daniel

 

0 项奖励
回复
4,083 次查看
kjy106906
Contributor IV

Thank you very much for your cooperation @danielmartynek 

Can you tell the difference between EVB and Internal Board?
Please check if there is any difference depending on the lot.

0 项奖励
回复
4,063 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

There no differences between lots.

The MCUs tested on all the boards: P32K312NHVPBS 0P09C

Have you tested the example I attached here?

 

BR, Daniel

0 项奖励
回复
4,026 次查看
kjy106906
Contributor IV

Thank you @danielmartynek 

Current consumption is normally reduced with your code.
I will check the difference between my code and yours.

4,106 次查看
kjy106906
Contributor IV

Thank you very much. @danielmartynek 
Is the S32K142 EVB a typo?
I also come out high current on custom boards.
I wonder if it's a problem with the MCU lot.
Can you share the top making of another NXP internal board?

0 项奖励
回复
4,097 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

@kjy106906,

What current do you measure on the custom board?

Is is ~350uA too?

 

Thanks,

Daniel

0 项奖励
回复
4,095 次查看
kjy106906
Contributor IV

@danielmartynek 

Yes, same as EVB.

Best Regards

Junyeong Kim

0 项奖励
回复
4,093 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

@kjy106906, would it be possible that you shared a schematic of your custom board?

You can share it privately via a ticket with reference to this thread.

 

Thank you,

Daniel

 

0 项奖励
回复
4,104 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, a typo, I just edited it, sorry for that.

Let me check.

The project tested is attached.

 

BR, Daniel

2,230 次查看
Akhil1
Contributor I

Hello @danielmartynek ,

Can you please provide code of S32k312 wakeup method using SBC FS26 using Long duration timer(LDT).

Regards

Akhil

0 项奖励
回复