S32K312 HSE FW Lost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
620件の閲覧回数
Shaun666
Contributor II

Hello,

I have been installed the HSE FW, and read HSE FW version succeed. 

image4.png

But when I program demo app again, I got a programming error as shown below picture, than I found the HSE installation state lost.

 there are a total of 3 ECU with same problem.  I don't know why. Is it possible for the HSE FW to be lost?

image7.png

Picture3.png

update to fix unclear picture

0 件の賞賛
返信
1 解決策
586件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry, there may be something wrong with the method you uploaded the picture, so I can't see the content of the picture clearly. Please click Insert Photo or attach those pictures.

Have you referred to MU Restore FW_EN.pdf in S32K312 HSE strange problem?


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
587件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry, there may be something wrong with the method you uploaded the picture, so I can't see the content of the picture clearly. Please click Insert Photo or attach those pictures.

Have you referred to MU Restore FW_EN.pdf in S32K312 HSE strange problem?


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
570件の閲覧回数
Shaun666
Contributor II
Thank you Robin,
I am sorry for unclear picture. I have been update it.
0 件の賞賛
返信
551件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

It looks like your S32K312's current SBAF Version(0x4039C020) is 01 0D 00 00 00 09 00 01. To make it fully compatible with SBAF, it is recommended to install HSE FW version 00 0D 00 00 02 06 00 00 or higher.

Which HSE_DEMOAPP are you using? HSE_DEMOAPP_S32K3XX_0_2_6_0 or the latest HSE_DEMOAPP_S32K3XX_0_2_40_0?

BTW, S32K312 SBAF 0.15.0 RTM Release is the latest version.

0 件の賞賛
返信
544件の閲覧回数
Shaun666
Contributor II
I am using HSE_DEMOAPP_S32K3XX_0_2_6_0 for first install ,and update the fw to the latest HSE_DEMOAPP_S32K3XX_0_2_40_0 succeed.
because SBAF programming during chip EOL, so we don't want to update it.
0 件の賞賛
返信