S32K1xx devices, Current timer value issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K1xx devices, Current timer value issue

ソリューションへジャンプ
425件の閲覧回数
wane
Contributor I

Hi,

At document 'S32K1xx Series Reference Manual, Rev. 13, 04/2020', 48.1.5 Current timer value, to read the register CVALn, it is recommended reading it during an LPIT interrupt service routine. Does this mean one of channel's ISR can read exact CVALs for other channel's? I want to manage the calibration of channel 1's CVAL at channel 0's ISR.

Regards,

0 件の賞賛
返信
1 解決策
395件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

No, it is still recommended to use the triple vote method to read CVAL. Please refer to the discussion: Tolerance of LPIT CVAL (Current timer value) 

Sorry for the inconvenience we bring you!

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
396件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

No, it is still recommended to use the triple vote method to read CVAL. Please refer to the discussion: Tolerance of LPIT CVAL (Current timer value) 

Sorry for the inconvenience we bring you!

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
377件の閲覧回数
wane
Contributor I

Thank you.

The triple vote method is working.

Regards,

0 件の賞賛
返信