Hi!
We are using the S32K148 with the RTD library but without the AUTOSAR Stack.
I am currently searching for an lwip example similar to the SDK RTM SDK lwip example.
Is there any implementation for an lwip under RTD without AUTOSAR?
Regards
Christof
Solved! Go to Solution.
Hi Christof,
It is included in the S32K1 Reference Software
Please read the release notes:
Regards,
Daniel
Hi Christof,
It is included in the S32K1 Reference Software
Please read the release notes:
Regards,
Daniel
Hi Daniel!
Thanks for your support.
Had to install the current version of the RTD via the Install Softwar option.
But it didn't work with the basic installation, after the setup of the S32 Design Studio.
Regards
Christof
Hi Daniel!
It seems that the installer is missing the RTD S32K1xx package, altlhough if have installed the whole RTD according to the update/install menu item.
Where can i get this item from?
Regards
Christof
Hi Daniel!
It doesn't work with the linstack either.
Must be some other stuff.
Regards
Christof
Hi Daniel!
Thanks for your fast reply.
Somehow the installation process does not work at my computer.
As mentioned in the release note I installed the FreeRTOS before I installed the TCPIP Stack.
But somehow this doesn't work as planened, after the installation I can't see the TCPIP Example.
There is only the one from the "old" SDK.
I already deinstalled/installed the package again and everytime it shows this message:
Can you give me a hint if I am missing some kind of package which I have to install in order to get the TCPIP Stack working?
Here is a screenshot from my installed packages.
Regards
Christof