S32K148, SD32DS, debugger launch takes lot of time.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148, SD32DS, debugger launch takes lot of time.

770件の閲覧回数
Vijay_Arwapally
Contributor III

I am using S32K148-EVB board. Initially the launch time of debugger was pretty fast.

But now the launch time as increased drastically. Like around 4-5mins.

Vijay_Arwapally_0-1611323316302.png

 

Can you let me know the reason for the same and how to decrease it?

0 件の賞賛
返信
2 返答(返信)

738件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Vijay_Arwapally,

Please refer: MultLink connect target with a long time
Hope it helps.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

727件の閲覧回数
Vijay_Arwapally
Contributor III

Suggested link has mentions to adding port numbers used by gdb in exception list of firewall.

The firewall application on my PC is controlled by Admin and I cannot modify or add exceptions to it.

 

Instead, everytime I delete the workspace and create a new workspace, the issue gets resolved.

Does it have anything to do with files that get stored in workspace area?

0 件の賞賛
返信