S32K146 downloading error in IAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 downloading error in IAR

Jump to solution
806 Views
sunnyfeng
Contributor II

Hello there,

I meet the following error when i download the S32K146 MCAL project in IAR.

 

 

Thu Aug 10, 2023 10:46:20: IAR Embedded Workbench 9.32.1 (C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm\bin\armPROC.dll) 
Thu Aug 10, 2023 10:46:20: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/config/debugger/NXP/KE1xF.dmac 
Thu Aug 10, 2023 10:46:20: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/config/debugger/NXP/S32K14x_trace.dmac 
Thu Aug 10, 2023 10:46:20: Flash download warning: 1636 out of 1636 bytes from data record CODE:[0x1fff'1380,0x1fff'19e3] will not be flashed 
Thu Aug 10, 2023 10:46:20: There were warnings while generating flash loader input. 
Thu Aug 10, 2023 10:46:20: See the Debug Log window for details. 
Thu Aug 10, 2023 10:46:22: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/config/flashloader/NXP/FlashS32Kxxx.mac 
Thu Aug 10, 2023 10:46:22: JLINK command: ProjectFile = C:\test_case\AUTOSAR\code\adwfs81218-autosar\TEST\settings\test_Debug.jlink, return = 0 
Thu Aug 10, 2023 10:46:22: Device "S32K146" selected. 
Thu Aug 10, 2023 10:46:22: DLL version: V7.88n, compiled Jul 26 2023 15:38:22 
Thu Aug 10, 2023 10:46:22: Firmware: J-Link V9 compiled May  7 2021 16:26:12 
Thu Aug 10, 2023 10:46:22: Selecting SWD as current target interface. 
Thu Aug 10, 2023 10:46:22: JTAG speed is initially set to: 1000 kHz 
Thu Aug 10, 2023 10:46:22: InitTarget() start 
Thu Aug 10, 2023 10:46:22: SWD selected. Executing JTAG -> SWD switching sequence. 
Thu Aug 10, 2023 10:46:22: InitTarget() end - Took 61.4ms 
Thu Aug 10, 2023 10:46:22: Found SW-DP with ID 0x2BA01477 
Thu Aug 10, 2023 10:46:22: DPIDR: 0x2BA01477 
Thu Aug 10, 2023 10:46:22: CoreSight SoC-400 or earlier 
Thu Aug 10, 2023 10:46:22: Scanning AP map to find all available APs 
Thu Aug 10, 2023 10:46:22: AP[2]: Stopped AP scan as end of AP map has been reached 
Thu Aug 10, 2023 10:46:22: AP[0]: AHB-AP (IDR: 0x24770011) 
Thu Aug 10, 2023 10:46:22: AP[1]: JTAG-AP (IDR: 0x001C0000) 
Thu Aug 10, 2023 10:46:22: Iterating through AP map to find AHB-AP to use 
Thu Aug 10, 2023 10:46:22: AP[0]: Core found 
Thu Aug 10, 2023 10:46:22: AP[0]: AHB-AP ROM base: 0xE00FF000 
Thu Aug 10, 2023 10:46:22: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM) 
Thu Aug 10, 2023 10:46:22: Found Cortex-M4 r0p1, Little endian. 
Thu Aug 10, 2023 10:46:22: FPUnit: 6 code (BP) slots and 2 literal slots 
Thu Aug 10, 2023 10:46:22: CoreSight components: 
Thu Aug 10, 2023 10:46:22: ROMTbl[0] @ E00FF000 
Thu Aug 10, 2023 10:46:22: [0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7 
Thu Aug 10, 2023 10:46:22: [0][1]: E0001000 CID B105E00D PID 003BB002 DWT 
Thu Aug 10, 2023 10:46:22: [0][2]: E0002000 CID B105E00D PID 002BB003 FPB 
Thu Aug 10, 2023 10:46:22: [0][3]: E0000000 CID B105E00D PID 003BB001 ITM 
Thu Aug 10, 2023 10:46:22: [0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU 
Thu Aug 10, 2023 10:46:22: Initializing 126976 bytes work RAM @ 0x1FFF0000 
Thu Aug 10, 2023 10:46:22: Reset: Halt core after reset via DEMCR.VC_CORERESET. 
Thu Aug 10, 2023 10:46:22: Reset: Reset device via AIRCR.SYSRESETREQ. 
Thu Aug 10, 2023 10:46:24: Reset: Halt core after reset via DEMCR.VC_CORERESET. 
Thu Aug 10, 2023 10:46:24: Reset: Reset device via AIRCR.SYSRESETREQ. 
Thu Aug 10, 2023 10:46:24: Hardware reset with strategy 0 was performed 
Thu Aug 10, 2023 10:46:24: Initial reset was performed 
Thu Aug 10, 2023 10:46:24: DMAC: Disable watchdog ... 
Thu Aug 10, 2023 10:46:24: ----- Prepare hardware for Flashloader ----- 
Thu Aug 10, 2023 10:46:25: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/config/flashloader/NXP/FlashS32K148RAM60K.out 
Thu Aug 10, 2023 10:46:25: Target reset 
Thu Aug 10, 2023 10:46:25: ----- Flush Caches ----- 
Thu Aug 10, 2023 10:46:25: Unloaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/config/flashloader/NXP/FlashS32Kxxx.mac 
Thu Aug 10, 2023 10:46:25: Downloaded C:\test_case\AUTOSAR\code\adwfs81218-autosar\TEST\Debug\Exe\test.out to flash memory. 
Thu Aug 10, 2023 10:46:25: 37868 bytes downloaded into FLASH (6.90 Kbytes/sec) 
Thu Aug 10, 2023 10:46:26: Loaded debugee: C:\test_case\AUTOSAR\code\adwfs81218-autosar\TEST\Debug\Exe\test.out 
Thu Aug 10, 2023 10:46:26: Reset: Halt core after reset via DEMCR.VC_CORERESET. 
Thu Aug 10, 2023 10:46:26: Reset: Reset device via AIRCR.SYSRESETREQ. 
Thu Aug 10, 2023 10:46:26: Hardware reset with strategy 0 was performed 
Thu Aug 10, 2023 10:46:26: Download completed. 
Thu Aug 10, 2023 10:46:26: Reset: Halt core after reset via DEMCR.VC_CORERESET. 
Thu Aug 10, 2023 10:46:26: Reset: Reset device via AIRCR.SYSRESETREQ. 
Thu Aug 10, 2023 10:46:26: Software reset was performed 
Thu Aug 10, 2023 10:46:26: Target reset 
Thu Aug 10, 2023 10:46:26: DMAC: Disable watchdog ... 
Thu Aug 10, 2023 10:46:26: There were 1 error and 1 warning during the initialization of the debugging session. 
Thu Aug 10, 2023 10:47:41: HardFault exception. 
Thu Aug 10, 2023 10:47:41: The processor has escalated a configurable-priority exception to HardFault. 
Thu Aug 10, 2023 10:47:41:  
Thu Aug 10, 2023 10:47:41:    An imprecise data access error has occurred (CFSR.IMPRECISERR, BFAR). 
Thu Aug 10, 2023 10:47:41:  
Thu Aug 10, 2023 10:47:41:    A derived bus fault has occurred on exception entry (CFSR.STKERR, BFAR). 
Thu Aug 10, 2023 10:47:41:  
Thu Aug 10, 2023 10:47:41: Could not determine the location where the exception occurred. 
Thu Aug 10, 2023 10:47:41:  
Thu Aug 10, 2023 10:47:41: See the call stack for more information. 
Thu Aug 10, 2023 10:47:43: IAR Embedded Workbench 9.32.1 (C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm\bin\armPROC.dll) 
Thu Aug 10, 2023 10:47:43: Loading the J-Link Driver driver 

 

 

Reproduce enviroment:

 

1. I'm using the SW32K1_RTD_4.4_1.0.1_HF01 MCAL source code

2. the linker file is inside the directory: SW32K1_RTD_4.4_1.0.1_HF01\eclipse\plugins\Platform_TS_T40D2M10I1R0\build_files\iar\linker_flash_s32k146.icf.

3. There is nothing in my main code only some init steps:

 

 

int main(void)
{
    /* Write your code here */
	Mcu_Init(NULL_PTR);
	Mcu_InitClock(McuClockSettingConfig_0);
	while (MCU_PLL_LOCKED != Mcu_GetPllStatus());
	Mcu_DistributePllClock();
	Mcu_SetMode(McuModeSettingConf_0);

	ResumeAllInterrupts();

	Port_Init( NULL_PTR );
	Platform_Init( NULL_PTR );

	Dio_WriteChannel(DioConf_DioChannel_EN_LOCK_MCU, STD_HIGH);
	Spi_Init( NULL_PTR );
	Gpt_Init(&Gpt_Config_VS_0);
    Gpt_StartTimer(GptConf_GptChannelConfiguration_GptChannelConfiguration_0, 10*20000000/1000);
	Gpt_EnableNotification(0u);

	int32_t err = 0;
    return err;

}

 

 

Could someone help me solve this issue? Or could someone give me an IAR project on s32k146 that using the MCAL source code as an example? I can not even run into the RESET_HANDLER in assembly and always get to the HardFault_Handler.

 

Thanks in advance!

 

0 Kudos
Reply
1 Solution
537 Views
sunnyfeng
Contributor II

Just to update my solution: Set the Entry symbol to Reset_Handler could solve this problem.

sunnyfeng_0-1709631438175.png

 

 

View solution in original post

0 Kudos
Reply
2 Replies
538 Views
sunnyfeng
Contributor II

Just to update my solution: Set the Entry symbol to Reset_Handler could solve this problem.

sunnyfeng_0-1709631438175.png

 

 

0 Kudos
Reply
671 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @sunnyfeng , 

Very sorry for late reply. 

Please can you check this post if the post is any help for you: 

https://community.nxp.com/t5/S32K/S32K-HardFault-exception/m-p/895372/highlight/true

 

Please let us know any update on the case. 

 

Thank you. Best regards. 

- Mehul Patel

0 Kudos
Reply