S32K146 LPUART TX issue with DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146 LPUART TX issue with DMA

365 次查看
chandan_uv
Contributor III

I am using S32K146 and using UART TX and RX with DMA. Its working fine most of time but sometime unable to tx as lpuart0_state.isTxBusy doesn't reset to false. As this is rarely occurring, I am unable to reproduce it for debugging. Below are the configuration for UART. Please let me know how to debug it. 

void init_uart(void){
	  status_t ret = STATUS_SUCCESS;

    lpuart_user_config_t lpuart1_cfg;
	
	  edma_init_iot_comm();

    lpuart1_cfg.transferType = LPUART_USING_DMA;
    lpuart1_cfg.baudRate = 1000000; 
    lpuart1_cfg.parityMode = LPUART_PARITY_DISABLED;
    lpuart1_cfg.stopBitCount = LPUART_ONE_STOP_BIT;
    lpuart1_cfg.bitCountPerChar = LPUART_8_BITS_PER_CHAR;
    lpuart1_cfg.rxDMAChannel = EDMA_CHN1_NUMBER;
    lpuart1_cfg.txDMAChannel = EDMA_CHN0_NUMBER;

    ret = LPUART_DRV_Init(UART_COM_4G, &lpuart0_state, &lpuart1_cfg);

    DEV_ASSERT(ret == STATUS_SUCCESS);
	
	  // setLpuartHardFlowCtrl();

    LPUART_DRV_InstallTxCallback(UART_COM_4G, lpuart_tx_callback_t, NULL);

    LPUART_DRV_InstallRxCallback(UART_COM_4G, lpuart_rx_callback_t, NULL);
	
	  LPUART_DRV_ReceiveData(UART_COM_4G, iot_rx_struct.data, MAX_RX_IOT_COMM_BUFFER);
		
		IOT_COMM_UART_FLOW_START_RX;
		
}
static status_t edma_init_iot_comm(void){
    status_t ret = STATUS_SUCCESS;
    
    edma_chn_state_t *const edma_channel_states[] = {
        &dma_ctrl_chn0_state,
        &dma_ctrl_chn1_state
    };

    edma_channel_config_t dm_chn0_cfg = {
        .channelPriority = EDMA_CHN_PRIORITY_1,
        .virtChnConfig = EDMA_CHN0_NUMBER,
        .source = EDMA_REQ_LPUART0_TX,
        .callback = NULL,
        .callbackParam = NULL,
        .enableTrigger = false
    };
    
    edma_channel_config_t dm_chn1_cfg = {
        .channelPriority = EDMA_CHN_PRIORITY_0,
        .virtChnConfig = EDMA_CHN1_NUMBER,
        .source = EDMA_REQ_LPUART0_RX,
        .callback = edma_RX_callback, //NULL,
        .callbackParam = NULL,
        .enableTrigger = false
    };
    
    const edma_channel_config_t *const edma_chn_cfg_arr[] = {
        &dm_chn0_cfg,
        &dm_chn1_cfg
    };

    edma_user_config_t dma_ctrl_init_cfg = {
        .chnArbitration = EDMA_ARBITRATION_FIXED_PRIORITY,
        .haltOnError = false
    };
    
    ret = EDMA_DRV_Init(&dma_ctrl_state, &dma_ctrl_init_cfg, edma_channel_states, edma_chn_cfg_arr, EDMA_CONFIGURED_CHANNELS_COUNT);  
    
		DEV_ASSERT(ret == STATUS_SUCCESS);
		
    return ret;
}

 

标记 (1)
0 项奖励
回复
3 回复数

328 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

hard to suggest here. I can give few hints only...
- be sure latest SDK version is used
- try to lower baudrate if possible and check, if issue appears too
- change DMA priorities over channels used
- when TXbusy is not reset, check within debugger internal state of lpuart driver and respective DMA channel (driver variable and module registers). Compare values with data sent, if any.

BR, Petr

0 项奖励
回复

212 次查看
chandan_uv
Contributor III

hI, I tried but still unable to find the issue. any other suggestion on debugging it ?

0 项奖励
回复

209 次查看
chandan_uv
Contributor III

Attaching resisters value during the issue

LPUART_0:

chandan_uv_0-1722594188779.png

 

DMA:

 

chandan_uv_1-1722594199937.png

 

chandan_uv_2-1722594209148.png

 

 

 

0 项奖励
回复