S32K144EVB-Q100 Factory Firmware and Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144EVB-Q100 Factory Firmware and Code

ソリューションへジャンプ
1,990件の閲覧回数
tpcom
Contributor II
Who can provide the download address for S32K144EVB-Q100 Factory Firmware and Code.
Thinks!
0 件の賞賛
返信
1 解決策
1,973件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi tpcom,

Do you mean the FreeMASTER JumpStart project mentioned in Get Started? If so, please refer to Q&A of S32K1x FreeMASTER JumpStart Project


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,974件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi tpcom,

Do you mean the FreeMASTER JumpStart project mentioned in Get Started? If so, please refer to Q&A of S32K1x FreeMASTER JumpStart Project


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,962件の閲覧回数
tpcom
Contributor II

Thank you very much Robin. I have found this program. In addition, there are independent programs for each peripheral device on this file “Document Number: AN5413 Rev. 0, 03/2017”. It is Application Note of NXP Semiconductors. Where can I download every code for the "Hello World ... CAN FD"?

tpcom_0-1663656256870.png

 

0 件の賞賛
返信
1,952件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Search AN5413, you will find the AN5413SW

タグ(1)
0 件の賞賛
返信
1,943件の閲覧回数
tpcom
Contributor II
The problem has been solved. Thank you very much for your support.
0 件の賞賛
返信