Hi Guys,
I created a FlexCAN program using "S32DS project from example" option from S32 Design Studio, ran that on the below evaluation board,
https://www.nxp.com/docs/en/quick-reference-guide/S32K144EVB-QSG.pdf
And I found no bit stream on PTE5 pin on the header pin J6-18.
Any idea?
Thanks,
Kevin
Hi,
you need to connect external 12V power supply to J16, so the SBC is powered and SBC's CAN transceiver becomes active. Without this CAN RX is kept low, so the FlexCAN module will not synchronize to a "bus" and will not transmit anything.
BR, Petr