Hi,
I'm working with s32k118evb. I can use on board OpenSDA debugger to download image and debug but the board doesn't work with PE Micro Multilink Universal FX.
I also have a s32k144evb board and this board works well with the same PE Micro Multilink device.
Can I use my PE Micro Multilink with this board?
Bruce
已解决! 转到解答。
Hi Bruce,
You can use PE Micro Multilink with this board.
From the photo it looks like J15 is not connected, but this jumper is used to power VDD_MCU. Please make sure the MCU is powered and try to debug it.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Bruce,
You can use PE Micro Multilink with this board.
From the photo it looks like J15 is not connected, but this jumper is used to power VDD_MCU. Please make sure the MCU is powered and try to debug it.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------