Dear sir,
Now I am using FlexIO to be 2 I2C masters with DMA. I will reset I2C1 master(DMA channel is 2 and 3) if it is always BUSY. And then I will do FLEXIO_I2C1_DRV_MasterDeinit() and then do FLEXIO_I2C1_DRV_MasterInit() to reset I2C1. Now I have a question is I should reset DMA(channel 2 and 3)? And if should, how to just reset DMA(channel 2 and 3)?
Thanks.
BR,
Sean Wu
Dear Sean Wu,
Why don't you use the FLEXIO_I2C_DRV_MasterTransferAbort()?
It also disables the DMA in FLEXIO_I2C_DRV_MasterEndTransfer().
Regards,
Daniel
Dear sir,
Thanks for your reply. Below are my steps to reset I2C1 when always busy. And you said DMA is disabled in FLEXIO_I2C_DRV_MasterTransferAbort(), and after reset I2C1, I should init DMA again?
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// FLEXIO_I2C_DRV_MasterTransferAbort(&i2cMasterState[0U]);
FLEXIO_I2C_DRV_MasterDeinit(&i2cMasterState[0U]);
FLEXIO_I2C_DRV_MasterInit(INST_FLEXIO_I2C_CONFIG_1, &Flexio_i2c_Config0, &i2cMasterState[0U]); //////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
Thanks.
BR,
Sean Wu.
Dear @seanwu,
There is no need to deinit DMA.
And I think there is no need to deinit the FLEXIO_I2C_DRV_Master either if you use the FLEXIO_I2C_DRV_MasterTransferAbort() function.
Regards,
Daniel
Dear sir,
So I just use FLEXIO_I2C_DRV_MasterTransferAbort() function to exit I2C Busy status?
I don't need to deinit/init DMA and FLEXIO_I2C_DRV_Master, right? And after FLEXIO_I2C_DRV_MasterTransferAbort() function, I can FLEXIO_I2C_DRV_MasterSendDataBlocking directly, right?
Thanks.
BR,
Sean Wu
Hi @seanwu,
This should be enough to restore the S32K1xx I2C Master.
But it can be BUSY because the bus is held low by the Slave device.
Refer to UM10204 I2C-bus specification and user manual
Section 3.1.16 Bus clear
https://assets.nexperia.com/documents/user-manual/UM10204.pdf
SW for reference:
https://www.nxp.com/docs/en/application-note/AN4803.pdf
tI2C_fault I2C_Restore()
Regards,
Daniel