Hi Sir:
IThe chip we use is S32K312,add the FlexCan RTD Driver ,it did not build success. More inform as below:
Tool:S3DS3.4
RTD:PlatformSDK_S32K3_2022_07 version:2.0.1
the error information as attachment picture error.jpg。
Thanks!
解決済! 解決策の投稿を見る。
Hi,Senlent:
Thanks for you reply.
I use the demo "FlexCAN_Ip_Example_S32K312" provided in RTD or New creat a project and remove the “compatibility.xml” file the error information (Newcreat.jpg),the demo error inforation (FlexCAN_Ip_Example_S32K312.jpg) as attachment picture.
Can you try to test the demo "FlexCAN_Ip_Example_S32K312" provided in RTD?
If this problem still exists,this may be a known bug of S32 DS V3.4 ,please try to remove the “compatibility.xml” located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration.
BR!
Can you provide the demo of "FlexCAN_Ip_Example_S32K312"?