S32DS PEmicro Connection Assistant

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS PEmicro Connection Assistant

1,062 次查看
Djuric
Contributor II

Hello,

Until recently I was able to debug code normally on my development board S32K3X4EVB-T172

with S32DS. All of a sudden, when I start the debugging process, I get this message PEmicro Connection Assistant, An error occured while connectiong to the interface

I updated the extension to the latest version but it doesn't help.

dubug.png

 

dbg.png

This message also started appearing:

2024-07-02_12h56_01.png

Literally everything was working normally until a few days ago....

Please help.

Thank you.

0 项奖励
回复
10 回复数

1,014 次查看
Djuric
Contributor II

Hello @Julián_AragónM ,


Thanks for your reply.
These three LEDs are on, you can see in the picture.

20240702_182802.jpg

I tried on another computer with no success.

I have Windows 11.

None of Xilinx aplications/drivers have been installed.

Is there any free SW tool I could use to erase the entire contents of the controller memory (except the S32DS)?

0 项奖励
回复

63 次查看
temp_user
Contributor I
How do you solve this issue finally? I met the same situation as well.
0 项奖励
回复

57 次查看
Djuric
Contributor II

I didn't solve it. The evaluation board is still bricked. I also tried with an external Cyclone debugger to access the chip through the JTAG 20 pin port. It is simply not possible to load SW to memory or erase ir. I think the problem is in FS26 chip that is stuck and I don't know how to get it unstuck.

0 项奖励
回复

994 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

I can see that LED D15 RST_OSDA is on. Also, neither D4 nor D5 are turned on.

Julin_AragnM_0-1719954007231.png

Please check if the either power supply is connected properly, or if the voltage level is lower that the specified [+12.0V to ≥2Amps].

NXP Does not provide SW tools for erasing the memory apart from S32DS, but you can look into third party, such as PROG Flash Programming Software or J-Link Flash.

Best regards,
Julián 

0 项奖励
回复

984 次查看
Djuric
Contributor II
The power supply that powers the board is fine. Paid tools such as PROG Flash Programming Software or J-Link Flash. are not an option for me right now.
0 项奖励
回复

939 次查看
Djuric
Contributor II
@Julián_AragónM I suspect the FS26 chip (in S32K3X4EVB-T172) is causing the problem. Do you have any way to restore it to default setting. Somehow to reset it, to enable normal functioning?
0 项奖励
回复

931 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

Below is a process for SPI commands to let FS26 enter normal mode. For your reference. 

Julin_AragnM_0-1720036168637.png

 

 

0 项奖励
回复

863 次查看
Djuric
Contributor II

@Julián_AragónM  and how exactly do you suggest I do this, given the fact that I can't connect to the microcontroller (EV board)?

0 项奖励
回复

811 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric

Sorry for the delay, does this issue also happens when a blank project is debugged? Do you have any debugging tool (PE Micro or J-link) to test the connection?

Please make sure the debug configurations are correct:

Julin_AragnM_0-1720639027504.png

Also, if you do not have HSE enabled, make sure the flash algorithm selection in Advanced Options is set correctly.

Julin_AragnM_1-1720639181955.png

Best regards,
Julián

 

0 项奖励
回复

1,018 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

Is the reset LED turned on? Could you possibly try to use the probe on different computer?

Have you installed in the meantime some other software on your computer (e.g. Xilinx)?

P&E Drivers for Windows utilize the 3rd party service Jungo WinDriver to enable USB support under windows 10. Xilinx also uses WinDriver for their driver packages, but older versions. Starting with the P&E Driver package 11.7, a conflict between P&E Drivers and software IDES that rely on older Jungo driver packages might occur.

Best regards,
Julián