S32DS PEmicro Connection Assistant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS PEmicro Connection Assistant

1,073 Views
Djuric
Contributor II

Hello,

Until recently I was able to debug code normally on my development board S32K3X4EVB-T172

with S32DS. All of a sudden, when I start the debugging process, I get this message PEmicro Connection Assistant, An error occured while connectiong to the interface

I updated the extension to the latest version but it doesn't help.

dubug.png

 

dbg.png

This message also started appearing:

2024-07-02_12h56_01.png

Literally everything was working normally until a few days ago....

Please help.

Thank you.

0 Kudos
Reply
10 Replies

1,025 Views
Djuric
Contributor II

Hello @Julián_AragónM ,


Thanks for your reply.
These three LEDs are on, you can see in the picture.

20240702_182802.jpg

I tried on another computer with no success.

I have Windows 11.

None of Xilinx aplications/drivers have been installed.

Is there any free SW tool I could use to erase the entire contents of the controller memory (except the S32DS)?

0 Kudos
Reply

74 Views
temp_user
Contributor I
How do you solve this issue finally? I met the same situation as well.
0 Kudos
Reply

68 Views
Djuric
Contributor II

I didn't solve it. The evaluation board is still bricked. I also tried with an external Cyclone debugger to access the chip through the JTAG 20 pin port. It is simply not possible to load SW to memory or erase ir. I think the problem is in FS26 chip that is stuck and I don't know how to get it unstuck.

0 Kudos
Reply

1,004 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

I can see that LED D15 RST_OSDA is on. Also, neither D4 nor D5 are turned on.

Julin_AragnM_0-1719954007231.png

Please check if the either power supply is connected properly, or if the voltage level is lower that the specified [+12.0V to ≥2Amps].

NXP Does not provide SW tools for erasing the memory apart from S32DS, but you can look into third party, such as PROG Flash Programming Software or J-Link Flash.

Best regards,
Julián 

0 Kudos
Reply

994 Views
Djuric
Contributor II
The power supply that powers the board is fine. Paid tools such as PROG Flash Programming Software or J-Link Flash. are not an option for me right now.
0 Kudos
Reply

949 Views
Djuric
Contributor II
@Julián_AragónM I suspect the FS26 chip (in S32K3X4EVB-T172) is causing the problem. Do you have any way to restore it to default setting. Somehow to reset it, to enable normal functioning?
0 Kudos
Reply

941 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

Below is a process for SPI commands to let FS26 enter normal mode. For your reference. 

Julin_AragnM_0-1720036168637.png

 

 

0 Kudos
Reply

873 Views
Djuric
Contributor II

@Julián_AragónM  and how exactly do you suggest I do this, given the fact that I can't connect to the microcontroller (EV board)?

0 Kudos
Reply

821 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric

Sorry for the delay, does this issue also happens when a blank project is debugged? Do you have any debugging tool (PE Micro or J-link) to test the connection?

Please make sure the debug configurations are correct:

Julin_AragnM_0-1720639027504.png

Also, if you do not have HSE enabled, make sure the flash algorithm selection in Advanced Options is set correctly.

Julin_AragnM_1-1720639181955.png

Best regards,
Julián

 

0 Kudos
Reply

1,028 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric,

Is the reset LED turned on? Could you possibly try to use the probe on different computer?

Have you installed in the meantime some other software on your computer (e.g. Xilinx)?

P&E Drivers for Windows utilize the 3rd party service Jungo WinDriver to enable USB support under windows 10. Xilinx also uses WinDriver for their driver packages, but older versions. Starting with the P&E Driver package 11.7, a conflict between P&E Drivers and software IDES that rely on older Jungo driver packages might occur.

Best regards,
Julián