Power supply from eva board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power supply from eva board

1,198件の閲覧回数
pietroserao
Contributor II

Good morning i have some questions.

 

I'm using a FRDMPK 144-Q100 S32k144 Evaluation board.

1) Can this microcontroller works with a 3.3V supply voltage?

2) Can i set the 3,3 V VDD voltage only using the evaluation board, without using external power supply?

    There is some setup?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,033件の閲覧回数
allen_willson
NXP Employee
NXP Employee

Pietro,

Yes this MCU can operate down to 2.7V

There is an unpopulated jumper at J10 which can allow to select between 3.3V and 5.0V. You'll need to remove the R64 which is a zero-ohm jumper that directly connects 5.0V to the micro - this needs to be removed so you can make a selection for 3.3V

Schematic attached.

#schematic

0 件の賞賛
返信

1,033件の閲覧回数
pietroserao
Contributor II

Thank you so much.

0 件の賞賛
返信