Power supply from eva board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power supply from eva board

1,066 Views
pietroserao
Contributor II

Good morning i have some questions.

 

I'm using a FRDMPK 144-Q100 S32k144 Evaluation board.

1) Can this microcontroller works with a 3.3V supply voltage?

2) Can i set the 3,3 V VDD voltage only using the evaluation board, without using external power supply?

    There is some setup?

 

Thank you.

Labels (1)
0 Kudos
Reply
2 Replies

901 Views
allen_willson
NXP Employee
NXP Employee

Pietro,

Yes this MCU can operate down to 2.7V

There is an unpopulated jumper at J10 which can allow to select between 3.3V and 5.0V. You'll need to remove the R64 which is a zero-ohm jumper that directly connects 5.0V to the micro - this needs to be removed so you can make a selection for 3.3V

Schematic attached.

#schematic

0 Kudos
Reply

901 Views
pietroserao
Contributor II

Thank you so much.

0 Kudos
Reply