I have been going through the RM to understand and read about clocks.
But one thing i don't get is:
I can't see any of this applied in the examples using SOSC and SPLL (clocks_and_modes.c)
When does this apply? Is it not important?
Hi,
I've a question regarding the topic.
Since I'm using 8 MHz externl crystal, I've configured the SCG_SOSCCFG[RANGE] = 10 (Medium frequency range selected for the crystal oscillator of 4 MHz to 8 MHz) even if the SPLL is selected as reference clock (SCG_RCCR[SCS] = 6 System PLL).
Every seems to work correctly.
What are the possible side-effect?
Is it a wrong configuration for RM 28.1.2?
Regards,
Carmelo
Hi Chris,
Please follow the reference manual.
The examples are rather simple.
Regards,
Daniel