No source available for "(gdb[21].proc[42000].threadGroup[i1],gdb[21].proc[42000].OSthread[1])

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No source available for "(gdb[21].proc[42000].threadGroup[i1],gdb[21].proc[42000].OSthread[1])

882件の閲覧回数
995094985
Contributor I

lpuart_echo_s32k144 

This project was changed to 64 pin chip. This error will occur when downloading flash.

It works when downloaded to RAM.

0 件の賞賛
返信
1 返信

870件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

I'm able to download this example with a 64 pin package option without any error into a flash (I have only 100 pin package of S32K144). I have used S32DS for ARM 2018.R1 and selected 64 pin package. Please, try to use the attached code.

 

I hope it helps.

Best regards,

Diana

0 件の賞賛
返信