Hi Community,
I am trying to merge two simple project in to one master project
Project 1 consist of the Addition function with int return.
Project 2 consist of the Structure variable where i want to store the Output.
In the Master Project i will call the Struct with its instance and variable to store the restul for e.g.
Instance.Result = Add(5,5); //execution in Master project
where....
Instance.Result is declared in the Project 2
Add(a,b) is declared in the Pojet 1
I am facing the issue of undefined struct is there any way to perform this operation.
Thanks & Regards
Nilkanth Vyas
Hi @VaneB ,
Thanks for the response. I merged two library in single project already i am struggling with structure incorporation in library.
want to define structure in library and then same struct want to access from the other project with inclusion of library but its not supporting.
Thanks & Regards
Nilkanth Vyas
Could you share how the two projects are linked to include the libraries?
Check the following post. It has information related to the topic that might be useful.
Link to Files and Folders in Eclipse
Managing Project and Library Dependencies with Eclipse CDT
B.R.
VaneB