LIN Question about S32K144EVB-Q100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LIN Question about S32K144EVB-Q100

1,475 次查看
jinhui_wu
Contributor III

I am testing LIN example in S32DS on S32K144EVB-Q100.

File->New->New S32DS project from example,then find S32K144 RTM SDK v1.0.0 Example Projects,open lin_master project.

builded ,complied,debuged,then un-plug USB cable.power on from 12V and reset the MCU.

I use Oscilloscope to look the wave of LIN pin and tx on TJA1027,I find wave is working.LIN is communicating.

Now I short LIN pin to GND for one second,at this time the wave of LIN pin lose,the wave of tx on TJA1027 lose.

when i don't short LIN pin to GND, LIN still can't work.

why?

after LIN pin is shorted GND for one second,then LIN pin isn't shorted GND.Would LIN still work as usually?

标签 (1)
0 项奖励
回复
0 回复数