Issue in setting Baudrate 921600 on Flexio UART for S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in setting Baudrate 921600 on Flexio UART for S32K144

Jump to solution
1,583 Views
mayureshp
Contributor II

Hello,

I am having issue in setting Baudrate for S32K144, in Design Studio. Whenever i set Baudrate to 921600, it automatically sets it to 1000000. Is it not supported by S32K?

I have attached an image showing roundoff of Baudrate on flexio UART

0 Kudos
Reply
1 Solution
1,566 Views
mayureshp
Contributor II

Ok Understood.

Its solved ..! Thank you

View solution in original post

0 Kudos
Reply
2 Replies
1,571 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi mayureshp,

Please try to switch the FlexIO peripheral clock source.

FLEXIO0_CLK.pngTable 27-9. Peripheral module clocking.pngTable 27-8. Peripheral clock summary (continued).pngActual Baudrate.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,567 Views
mayureshp
Contributor II

Ok Understood.

Its solved ..! Thank you

0 Kudos
Reply