Hello,
I am having issue in setting Baudrate for S32K144, in Design Studio. Whenever i set Baudrate to 921600, it automatically sets it to 1000000. Is it not supported by S32K?
I have attached an image showing roundoff of Baudrate on flexio UART
Solved! Go to Solution.
Hi mayureshp,
Please try to switch the FlexIO peripheral clock source.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Ok Understood.
Its solved ..! Thank you