Issue in setting Baudrate 921600 on Flexio UART for S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue in setting Baudrate 921600 on Flexio UART for S32K144

ソリューションへジャンプ
1,584件の閲覧回数
mayureshp
Contributor II

Hello,

I am having issue in setting Baudrate for S32K144, in Design Studio. Whenever i set Baudrate to 921600, it automatically sets it to 1000000. Is it not supported by S32K?

I have attached an image showing roundoff of Baudrate on flexio UART

0 件の賞賛
返信
1 解決策
1,567件の閲覧回数
mayureshp
Contributor II

Ok Understood.

Its solved ..! Thank you

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,572件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi mayureshp,

Please try to switch the FlexIO peripheral clock source.

FLEXIO0_CLK.pngTable 27-9. Peripheral module clocking.pngTable 27-8. Peripheral clock summary (continued).pngActual Baudrate.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,568件の閲覧回数
mayureshp
Contributor II

Ok Understood.

Its solved ..! Thank you

0 件の賞賛
返信