How to startup communication from S32k148 MCU to SBC in S32k148evb board q176pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to startup communication from S32k148 MCU to SBC in S32k148evb board q176pin?

643 次查看
young_man
Contributor I

NXP was said in order to startup the communication in UJA1132 with SPI,we must remove thw R177 and R154 .So how do this used to jumper lines?

0 项奖励
回复
3 回复数

629 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@young_man

Can you tell me where you got this from, I need to check if this information is correct

0 项奖励
回复

615 次查看
young_man
Contributor I

I bought a board of S32K148EVB-Q176 .

The board SCH is S32K148EVB-SCH-29644-RB and another question is SBC type is UJA1131F5v0 on board ,but one is UJA1132F5v0 in S32K148EVB-SCH-29644-RB.

And set SPI  communication from MCU to SBC with read UJA113X_SER,the pdf said  ''During a write operation, the UJA113x monitors the number of SPI bits transmitted. If the
number recorded is not 16, 24 or 32, the write operation is aborted and an SPI failure
interrupt is generated (SPIFI = 1), if enabled (SPIFIE = 1).
 '',that means frame buffer must be 16bits transmission or buffer is 8bits frist frame and need second 8bits frame to startup SBC(1131/2).

 

0 项奖励
回复

604 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi,

I don't quiet understand your question,if you want to communicate with SBC,you can take a look the demo provided in S32 DS,I attached it for your reference.

Senlent_0-1679539599483.png

 

0 项奖励
回复