Hi
I am currently working on S32 Design Studio v2.2 , my need is to work with SDK RTM1.0.0 , My controller part is S32K144EVB. I Searched in whole community no where i found the answer. I did chat with community also, they are saying raise a ticket here, so i am requesting you to provide Download link for SDK RTM 1.0.0 with .xml file for S32 DS ARM. if this combination is not there, suggest better RTM version for S32 DS ARM.
Thank you
Hi @NadipalliLTTS,
The SDK RTM 1.0.0 version is very old (released in Apr 2017), it was a part of S32DS 1.3 if I'm not mistaken.
Why do you need this version?
In S32DS 2.2, there is SDK RTM 3.0.3 - the lastest version with the Processor Expert GUI.
BR, Daniel
I downloaded S32DS_ARM_v1.3_Update2_b170419(have RTM 1.0.0) from Downloads
my problem solved. Thank u team for the reply